Version confusion

Moderators: lily.li, salmanfarisvp, violet, jeremy882, crail.lyu969

Post Reply
runtrain
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sat Jan 09, 2010 7:22 am

Version confusion

Post by runtrain » Fri Jan 15, 2010 11:18 pm

Had my Nano for a week and have been studying the posts on this board.

I have question about versions:

When turned on, startup screen reads
Nano v. 1.1 (at top)
firmware version 2.02 (at bottom)


Circuit board edge near battery reads
DSO201V1.3A

What versions do I have? I am confused trying to decide what comments apply to my device.

I purchased my Nano from NKC Electronics in the US two weeks ago.

Thank you very much for any help

FreeZinG

Re: Version confusion

Post by FreeZinG » Sat Jan 16, 2010 12:53 am

Nano v. 1.1 (at top) : The DSO Nano version (model)

firmware version 2.02 (at bottom) : the firmware version

DSO201V1.3A : the hardware version

runtrain
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sat Jan 09, 2010 7:22 am

Re: Version confusion

Post by runtrain » Sat Jan 16, 2010 8:24 am

Thanks. Now I think I know where I am.

So far, I think I have

1) file reading/saving with SD disk working
2) DSO recognized by 3 Dfuse software programs

Next steps are to try upgrading firmware.

Also, not sure about best procedure for charging battery - in device or remove and use separate Li Bat charger?

FreeZinG

Re: Version confusion

Post by FreeZinG » Sat Jan 16, 2010 8:50 pm

The safest way is the charge circuit of cause, but it also has some issues .the circuit now is also acceptable and really work in most simplicity MP3,MP4 machine.

davidea
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Tue Jul 13, 2010 5:20 am

Re: Version confusion

Post by davidea » Wed Jul 14, 2010 7:13 am

FreeZinG wrote:Nano v. 1.1 (at top) : The DSO Nano version (model)

firmware version 2.02 (at bottom) : the firmware version

DSO201V1.3A : the hardware version

sorry, but i don't understand......whic difference between

The DSO Nano version (model)

and

firmware version 2.02 (at bottom) : the firmware version

in my unit (an e-design unit, but don't worry, i know you after i've buied the unit! :-( )

at startup i've only

version 1.5.20P ( i think paul version 1.5.20), is then all ok?
for knowing the hardware version i must open the back panel?

User avatar
esp
Elementary-3
Elementary-3
Posts: 361
Joined: Fri Aug 22, 2008 5:45 pm

Re: Version confusion

Post by esp » Wed Jul 14, 2010 9:29 pm

You could try different firmware on any version whenever needed.

Check it out here: code.google.com/p/dsonano/

Post Reply