To clarify there were three issues that had confusingly similar results.
Using Windows 8.1 I had loaded without issue at least 10 different APP files including all the Wildcat versions up to and including 4.3 and they just worked with no problems I was aware of. It made no difference I had noticed extracting the file first or copying direct from the archive, remembering this is something done once every few weeks.
Wildcat 4.4 would not load no matter what I tried using Windows 8.1 and I have now found by experiment that there is a size somewhere between Wildcat 4.3 and 4.4 beyond which Windows 8.1 will not successfully copy to the DFU. Windows 8.1 shows no error when this fails and confusingly the DFU often shows the file as .RDY as if it had successfully loaded when it had not. It is easy in hindsight to see the file size was a problem for copying but at the time it looked more like the DFU was not loading the file correctly because of undocumented size constraints on app slots.
After trying to load Wildcat 4.4 the only thing working was the DFU and the splash screen when trying to start the APP was corrupted and no version of the APP would successfully load via Windows 8.1.
After a lot of trying SYS 1.64 fixed the corruption on the splash screen and allowed an early version of the app to load but the software crashed whenever the 8MB drive was mounted which looked like a corrupted config file. For whatever reason SYS 1.64 would also not allow Wildcat 4.4 to load.
I built a Windows 7 box and tried the test app’s Wildcat had but to bypass loading the config file with no success. Went back to 1.62 which would not load under windows 8.1 but loaded successfully with Windows 7 and found that 1.62 allowed the 8MB volume to load.
With Windows 7 I could use all apps up to Wildcat 4.3 and PAWN worked for the first time but no version of 4.4 would run. By this stage I had started downloading a fresh version of the APP for each test in case there was some corruption, then opening the archive and copying to the DFU volume. I did not give it any thought because it had never caused problems before and was supposed to be kosher according to Microsoft. It was only when the contiguous test version of 4.4 was taking over 3 minutes to copy and fail I started thinking something was broken in the copying process rather than the hex parsing and flash write on the DFU side.
It was very confusing going from a full working Wildcat 4.3 with no previous problems to a completely broken setup after loading 4.4 with nothing different other than the version of Wildcat.
Things learnt:
Use Windows 7 or XP to load files.
Extract files before copying to the DFU volume
Don’t use SYS 1.64 if it did not come setup that way, it may cause problems with mounting the 8GB drive. SYS 1.62 works well with windows 7.
Windows 8.1 may corrupt the default config file when mounting the drive.
Windows 7 sometimes glitches when the DFU drive disconnects and reconnects after loading. Manually disconnect and reconnect the USB cable and check if the file is marked .RDY usually it will have loaded successfully, powering off and on can also help.
It is worth sorting out the issues as Wildcat 4.4 is excellent and transforms usability compared to the stock application.
First of all I want to say big thanks to Wildcat and all people who help make this great job. The Best Firmware I believe.
And I want to report that I upgrade successfully to 4-slot firmware W4.4 from p.41 on 2.81 DSO. But only on Windows 7 PC.
When I tried to do it at w8 or w10 I either did not get any result, either I erase all and I had to completely reflash all (sys, fpga, etc.) on the W7 PC. Is is so and for another hex files (other versions).
And one question for Wildcat:
How many periods is necessary for the frequency counter in meters? I get result only from 4…5 if I try adjust xpos, and at least 10 for stable.
I don’t believe it can be done but just in case I missed something – Is there a way to plot frequency over time (ie, a histograph?) with Wildcat’s firmware?
It’d be cool if you could take the frequency of some input and represent it as a graph vs time. Sometimes it’s easier to see glitches this way-overshoots and undershoots from a sensor- vs. just looking at the waveforms.
Wildcat, just tested this version on my dso, this one copies 3/4 before disconnecting and manages to write some data leading to the attached boot screen. You seem on the right track as the versions before only copied like 2/4 before disconnecting in the middle of the copying operation. Also this version seemed to overwritten PAWN while the v4.4 “3-slot” and “reduced rom + ram” which install fine don’t overwrite PAWN.
edit: open the attachment image in new tab as it does not re-scale properly in the forum
DID IT! I updated my hw v2.81 to DFU v3.45C and activated with my license key! Now the DFU drive works in Windows 10!
Also Wildcat i tested your v4.4 (4-slot version, + v2.81 v4.4 test version) and they still don’t work. “3-slot” version, “reduced rom + ram” + pawn still work perfectly.
I will be making a tutorial on flashing DFU so stay tuned:)
Look, it seems you are confusing two different problems. DFU drive support in Windows 8/8.1/10 is one problem, which has been now fixed with DFU v3.45C. The second problem is installing your v4.4 "4-slot" version in hw v2.81 devices. This done under XP/7/10 will fail due to how you wrote your program. It has nothing to do with the OS. I wished i had the money to buy you a hw v2.81 so you could develop on but seeedstudio/minidso they should at least send you one for free for your efforts!
edit: Flashing tutorial is up! http://www.seeedstudio.com/forum/viewtopic.php?f=26&t=6186
Hi, I have Hardware 2.81 with MCU Type STM32F103VE Running:
DFU 3.40C
SYS1.62
APP is Wildcat 4.4 from Page 41 and
PAWN ver 0.11
SYS, APP and Pawn can be loaded with no errors using Windows XP or Windows 7
The APP 4.4 stops loading every single time under Windows 8.1
The 4.3 APP can occasionally be loaded successfully under Windows 8.1 but loads every time under Windows 7
My understanding for this combination of 2.81 hardware and 3.40C DFU is the errors are related to the size of the file and Windows 8.1 failing to load to the DFU volume, not the arrangement of APP slots used.
It is possible with a newer DFU that Windows 8.1 might load 4.4 without errors but the DFU 3.40C Window 8.1 problem is one identified by the support team for the authors of the DFU.
I don’t think the errors loading the file are anything to do with Wildcats 4.4 APP other than the size exceeds what ever limit causes loading to fail under Windows 8.1 and DFU’s 3.42 and below. USE Windows 7 and 4.4 loads and runs (either version) remembering the version on page 41 allows space for PAWN.
I have spent days on this, I could be wrong and please do your own tests. If someone had told me before Wildcat 4.4 was available “Only use Windows XP or 7 when loading APP’s and SYS files” I would have 30+ hours of my life back.
I am still very happy because Wildcats 4.4 in my view is well worth the time I spent to get it working, especially if it helps other people avoid the swamp.
Hi, I would not be confident DFU version 3.45C has resolved APP loading issues with Windows 8.1 and 10 until this was tested carefully.
Wildcat 4.4 is the largest APP yet written for this platform and was not available for testing when DFU 3.45C was written. My understanding is it was written to address flakey copying of 2 and 3 slot applications and possibly allow Mac OS to copy files.
The 8MB volume supposedly needed at least SYS 1.64 to work with Mac OS but SYS 1.64 can cause other problems with crashing at launch.
Again I can only test what I have and I agree someone, probably SEEED? should sent Wildcat several units with 2.81 hardware and DFU 3.40C and on a second unit the latest shipping version.
On the last note yes i too believe Wildcat should be sponsored a hw v2.81 unit at least.
Regarding testing, DFU v3.45C has been around for a couple of months already, and did my testing too on Windows 10, and there are no disconnection problems. On the other hand the large .hex app file disconnection issue could be either workaround in the app software by Wildcat or either in the DFU but let’s be honest, how many people would open the device and flash using an RS232 adapter?
TheNaughtyFantasy Hi, I agree many may avoid serial flashing but thanks to your DFU adventure and file archive upgrading is at least doable, I certainly will give it a go.
One reason I have been more inclined to think large APP (4.4) + Windows 8.1 is causing issues is my cheese and chalk experience loading the same files on Windows 7 VS 8.1
There is no doubt the APP still has to sit inside the boundaries of available/legal flash but I believe version 4.4 - the page 41 version does this. Hopefully DFU 3.45C is golden but I would not be surprised if it took another revision to get it behaving with these very large APP sizes and Windows 8.1/10.
Do you think it’s worth us each PayPal-ing $5-10 to Wildcat to buy the new version?
In regard to the disconnection problems not seen in Windows 10, in Windows 8.I never saw disconnections using the DFU, in fact it almost always seemed like thinks were ok and files would often load and show .RDY but still be not loaded properly (they showed .ERR regularly as well). If I can load Wildcat 4.4 using Windows 7 and everything is working my belief is that code is good. We do need a way of loading large APP’s reliably with Windows 8.1 and 10 and that might involve a new DFU version for something as big as 4.4 - perhaps we should get whoever wrote DFU 3.45C to test it out and see if it is possible. Whatever - your point about the users not re-flashing their DFU is bang on and they will not want to buy new hardware to get the new DFU either so perhaps some clever code that loads as an APP and then updates the DFU might do it, or be impossible for whatever reason. Perhaps SEEED could consider selling the right serial cable setup ready to go to help users update. It may to be a bigger nose bleed for many users to get Windows 7 or XP happening than refresh their DFU if a version that makes it all wonderful is available, perhaps with a script that backs up everything first and allows recovery without skillz.
Awesome. That’s what I thought the Spectrograph function was for. But when I used I had always gotten a vomit of colors and figured it was a different type of spectrograph than what I was hoping for. Anyway, it works. I will need to tinker with this a bit and delve into the manual.
That’s the weird thing…in my device even under windows 7 v4.4 “4-slot” version will not install. Anyways i’m planning to test all of the versions from v4.1 + test versions again with sys 1.62 + sys 1.64 and make a list of what works and what doesn’t.
We could make some paypal crowd funding but it’s better to make a thread first so that we gather more people and so the seeedstudio sees it and hopefully helps us a bit.