installing some software on the DSO Quad is much more simple than you might think (and is explained in this thread (first message - which I quote after the link - but just read the general procedures after the quote):
You can do all that upgrading or softwarechanging, after you connect the DSO Quad to your PC via USB and while turning on the DSO Quad, pressing the first button "►||" on the left of your DSO Quad. (It will then show up as a drive on your PC)
--> The firmware/software for the DSO Quad consists of 4 things:
[list]
FPGA
[/list] [list]
APP
[/list] [list]
SYS
[/list]
and if you wish [list]
logo
[/list]
the FPGA and the logo consists of 2 Files each: you first have to “send to” or “copy/paste” into the DSO Quad drive a / the “xxx.ADR” file followed by the matching “xxx.bin” file
–> “xxxFPGAxxx.ADR” and the “xxxFPGAxxx.bin” for the FPGA and “xxxlogoxxx.ADR” followed by “xxxlogoxxx.bin” for the Logo
APP and SYS are “xxx.hex” files and for those, you only “send to” or copy/paste a/the “xxx.hex” files to the DSO Quad drive - the DSO Quad then automatically reboots and reconects with your PC, showing a “xxx.rdy” file on the DSO Quad drive.
The combination of FPGA, SYS or the APP is what seems to be an issue, as all have been updated several times and based on on or the other code, SYS and APPs have been improverd or developed - but there is not much that can happen to the DSO quad
I remember having this same problem. Please check that you have the latest Marcosin SYS file. See the sticky post on this thread which explains what you need.
Thanks for your excellent work on this build (v1.21). One minor bug that I have not been able to sort out.
When triggering from Chan A, on manual, down transition, 2ms per div, it works perfectly on full buffer mode, but when I switch to short buffer mode, it appears to trigger OK about one sweep in 3 or 4, and then free-run for the next 2 or 3 sweeps.
If you have any ideas where I might look in the code, I’m happy to try to sort it out, but I’m not sure where to look to start with.