I wish to have a low speed signal recorder function for making battery discharge voltagedrop tests.
Battery discharge test take several hours.
The current 1s/div is far too fast for this kind of testing.
Then I need to take a bitmap of the displayed waveform.
This should be rather easy to implement for everybody with a minimal experience in software engineering.
I suggest you have a look at Petteri Aimonen’s page essentialscrap.com/dsoquad/freq.html, his “frequence response application” is an excellent starting point and very well commented. His instructions about how to install a freeware development environment on Windows are easy and they work (not like others here…).
i m watching the sources of DSO_gcc_v7.1 and have different questions…after 2 min of watching.
why do you still poll in timer handler the keyboard state(keys pressed), and don’t have keyboard interrupt, as any good hardware? what a strange idea - permanently poll rare events, if interrupts make it easy and in proper way.
Hi! I need help.
My device gives out the wrong form of a signal on the channel “A”. I repeatedly changed an firmware, the result on all is identical. I understand that malfunction is not in the program, and in the hardware. I ask to prompt to me, what details on a payment can be faulty?
I changed the probes, it didn’t solve a problem.
On a screenshot both channels (A and B) are connected to the same signal, only shifted for the period
I assume your input signal is square wave. Try adjusting the trimmers behind the battery - it may help. Looks like too much reactance compensation on Ch A and too little compensation for Ch B. This page has instructions:
No, in the channel “B” the true form of a signal is shown. It is checked for 100 % a serviceable oscillograph. It is a signal on the power unit of the amplifier (the enclosed file) in the points noted red. Many thanks for the reference, I will try according to your recommendation and I will report about results.
Heh, in the past 9 months, never has Seeed or eDesign co. fixed a single bug properly. There have been some updates, but the horrible triggering bugs and malfunctioning calibration remain as ever.
Hehe, surprisingly I wouldn’t return the device even if I could. As a portable oscilloscope, with all its defiencies, it’s still the best one I’ve ever owned. The typical 10 MSps multimeter-style devices with grayscale screens and no programs are nothing compared to the Quad.
Hi jpa.
I read your post about this problem related by kabron; maybe we can do the trick you used in your logic analizer program into the community app ?
I have the same issue. After calibrating the DSO like 4 times, I cannot get a clear measure from a power supply at 5V. I always get ~1.8V difference, and what is worse, it seems to change after each restart.