ReSpeaker Core v2 & 4-Mic Linear Array for Raspberry Pi

Can't find a proper forum to drop the topic, drop here.

Moderators: lily.li, violet

Post Reply
miguel.karpf
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Wed Sep 12, 2018 5:09 pm

ReSpeaker Core v2 & 4-Mic Linear Array for Raspberry Pi

Post by miguel.karpf » Mon Oct 01, 2018 7:17 pm

Hello,

I am using the ReSpeaker Core v2. Can I connect the 4-Mic Linear Array Kit for Raspberry Pi to it?

As far as I see I2C connection is available but I do not have the 40 Pin raspberry header.

Further I need to exchange the FFC cable, 20cm are not enough for my application. Is there a MAX length? I could not find these information...

Thank You,

Miguel

bill.yu
Junior-7
Junior-7
Posts: 732
Joined: Mon Apr 02, 2018 11:05 am

Re: ReSpeaker Core v2 & 4-Mic Linear Array for Raspberry Pi

Post by bill.yu » Fri Nov 02, 2018 6:07 pm

Hi Miguel

The respeaker core v2.0 integrates the mics. why do you plan to attach the mic pi hat?

for the FFC cable, here is the datasheet for the cable, you shall be able to find it from internet. thanks.
30Pins, 0.5mm distance

https://www.amazon.com/30-pin-Forward-D ... 30+pin+ffc

Post Reply