we want to use your Display with manufacture number 104060007 in our Product

Can't find a proper forum to drop the topic, drop here.

Moderators: lily.li, violet

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Tue May 21, 2019 8:28 pm

Hi,
we want to use your Display with manufacture number 104060007 in our Product. We bought one for the Prototype. In the data sheet it say it has a resolution of 1024 x 600. The one we got has a resolution of 1280 x 720. My Question now is, if we later use the product in manufacturing, which resolution does it have?

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Wed May 22, 2019 5:55 pm

Hi there,

It is 1024 x 600, Which device do you connect the LCD to? How do you configure 1280 x 720?   

Thanks

best rgds
Bill


Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Thu May 23, 2019 3:29 pm

Hi,

at the moment we are using the Banana Pi M2 Berry.
It doesnt even give us the possibility to change the resolution. The Native
resolution there is 1280 x 720 and can't be changed.

When i connect the Display to a Computer, then i can change the resolution.
There it is showing me the native resolution is 1024 x 600, but i still can
choose 1280 x 720.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Thu May 23, 2019 4:04 pm

Hi there,

I talked with designer that he also does not use with Banana Pi before. We do not have the banana pi on hand. We only test with raspberry pi and windows/mac. Thanks for understanding. 
 For raspberry pi, we config the 

resolution from below instructions. I am not if banana pi has the same configuration. 
Login to your Raspberry Pi and edit /boot/config.txt file, make sure it has following parameter:hdmi_force_hotplug=1 hdmi_group=2 hdmi_mode=87 hdmi_cvt 1024 600 60 3 0 0 0Save it and reboot your system.  Thanksbest rgdsBill

Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Thu May 23, 2019 4:30 pm

Hi Bill,

thank you for the infos.
We will check the configs later. Due to time management we will at first
use the resolution of 1280 x 720 since it is working.
Later on for future prototypes and batch production we will check if we
need to change the resolution, or if it is working good this way.

Post Reply