Page 1 of 1

Running Linkitone from an External Battery

Posted: Thu Mar 31, 2016 9:03 pm
by tflora15146
Does anyone see a problem with running the Linkitone from the USB port with a 5v source.
This is for an automotive application. I can convert the 12v car battery to 5v using a buck converter to a modified USB cable to provide power only to the micro USB port.

Re: Running Linkitone from an External Battery

Posted: Mon Apr 04, 2016 4:40 pm
by viswa
Hello,

If you are powering the LinkIt ONE board via micro USB port using 5V, it would be fine. Please make ensure the polarity (i.e +5V and Ground of USB Cable).

Thanks and Warm Regards.