I would like to run my Linkitone from a 12v Battery in order to reduce the voltage I have a 5v 3A UBEC DC/DC (Buck) converter.
The battery input on the spec sheet says 4.2V.
The question is:
What is the upper voltage limit on the battery port.
Running Linkitone with 5V 3A UBEC
Moderators: lily.li, violet, salmanfarisvp
-
- Pre-kindergarten
- Posts: 2
- Joined: Sat Mar 26, 2016 7:35 am
Re: Running Linkitone with 5V 3A UBEC
The upper voltage limit is 4.2V.