dimension & schematics of the Arduino Breakout

Moderators: lily.li, violet, salmanfarisvp

Post Reply
rva
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sun Jan 10, 2016 6:53 pm

dimension & schematics of the Arduino Breakout

Post by rva » Mon Jan 25, 2016 5:55 pm

Do you have the dimensions and schematics of the Arduino Breakout , location of the holes etc..

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: dimension & schematics of the Arduino Breakout

Post by kavi » Mon Jan 25, 2016 8:08 pm

Dimension is 107.32mm*53.34mm and eagle schematics are available in the following wikilink.

Thanks and Regards

rva
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sun Jan 10, 2016 6:53 pm

Re: dimension & schematics of the Arduino Breakout

Post by rva » Fri Feb 12, 2016 10:25 pm

This is very usefull but for a 3D project we need the exact location of the screw emplacement on the board (to build a 3D printed support) and so we need to have a schematics with a correct scale (or scale on it) ..

Post Reply