Question about LinkIt ONE wifi security

Moderators: lily.li, violet, salmanfarisvp

Post Reply
matthew
Pre-kindergarten
Pre-kindergarten
Posts: 27
Joined: Mon Dec 29, 2014 2:11 pm

Question about LinkIt ONE wifi security

Post by matthew » Fri Mar 20, 2015 6:34 am

LinkIt ONE has wifi security option of WPA, is this WPA or WPA2 or both?
if it is really WPA2 does it use AES security?

chinak2001
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Apr 10, 2015 5:26 pm

Re: Question about LinkIt ONE wifi security

Post by chinak2001 » Fri Apr 10, 2015 5:40 pm

Thanks matthew for bringing this up.
I faced the same challenge getting the LinkIT ONE to connect to my router at home which uses WPA2-Personal.
I had to change the Encryption to TKIP as AES seems to present challenges.

Also i got an error regarding the m_password variable in one of the files being null - but it still worked in the end.
If they can fix these little teething issues - i think this is really the board to use.

It is totally brilliant.

Post Reply