LinkIt ONE has wifi security option of WPA, is this WPA or WPA2 or both?
if it is really WPA2 does it use AES security?
Question about LinkIt ONE wifi security
Moderators: lily.li, violet, salmanfarisvp
-
- Pre-kindergarten
- Posts: 3
- Joined: Fri Apr 10, 2015 5:26 pm
Re: Question about LinkIt ONE wifi security
Thanks matthew for bringing this up.
I faced the same challenge getting the LinkIT ONE to connect to my router at home which uses WPA2-Personal.
I had to change the Encryption to TKIP as AES seems to present challenges.
Also i got an error regarding the m_password variable in one of the files being null - but it still worked in the end.
If they can fix these little teething issues - i think this is really the board to use.
It is totally brilliant.
I faced the same challenge getting the LinkIT ONE to connect to my router at home which uses WPA2-Personal.
I had to change the Encryption to TKIP as AES seems to present challenges.
Also i got an error regarding the m_password variable in one of the files being null - but it still worked in the end.
If they can fix these little teething issues - i think this is really the board to use.
It is totally brilliant.