Terrarium controled by Linkit ONE

Moderators: lily.li, violet, salmanfarisvp

Post Reply
back_kevin
Pre-kindergarten
Pre-kindergarten
Posts: 14
Joined: Sat Dec 06, 2014 7:07 am

Terrarium controled by Linkit ONE

Post by back_kevin » Wed Mar 11, 2015 1:44 am

HI here is my new project :

controle my terrarium with Linkit ONE:

features:
-control the water in the tank (if to low switch all water tools off)----------------------------------in progress
-control the humidity (if over 70% switch foger off )-----------------------------------------------ok
-control light (switch light on at 6h00 and off at 23h00)--------------------------------------------ok
-control Temp (if under 30°C switch heaters on if over 35°C switch off)----------------------------ok
-control Heater (if temp over 45°C switch off under 30°C switch on)-------------------------------ok
-control rain (set the rain interval to 2h raining delay to 2 min)-------------------------------------ok
-control LCD (2 lcd displays to show infos)---------------------------------------------------------ok
-SD Data logger------------------------------------------------------------------------------------ok
-html display page (show infos in Auto and in Manu mode switch different outputs )----------------in progress

material:
1* Linkit ONE
1* Grove shield
2* I2C LCD Display 20*4
2* Temperature and Humidity Sensor Model:SEN11301P
2* Temperature Sensor
1* IR Distance Interrupter
5* Screw Terminal Model: COM12533P
1* Tinty RTC Clock I2C
1* Relais board I2C (my board with Pcf8574)
1* SD card 16GB (for Data logger)

Bugs:
-Wifi stop some times
-can`t switch from auto to manu from html
-in Manu mode after bp is clicked -> page reload -> Output is Set -> page show old stats
-all values must be change in the sketch (later over html)


i hope you like ;)
Last edited by Jacket Chen on Tue Mar 17, 2015 11:17 am, edited 1 time in total.
Reason: +10 points. Thanks for your share.

User avatar
loovee
Elementary-3
Elementary-3
Posts: 352
Joined: Fri Nov 02, 2012 9:15 am

Re: Terrarium controled by Linkit ONE

Post by loovee » Tue Mar 17, 2015 11:09 am

Nice project!
There's such a fish tank in Seeed office, see if someday I can make it our and place there.

One more question, will you share it to Recipe(http://www.seeedstudio.com/recipe/) let more guys to make one?

back_kevin
Pre-kindergarten
Pre-kindergarten
Posts: 14
Joined: Sat Dec 06, 2014 7:07 am

Re: Terrarium controled by Linkit ONE

Post by back_kevin » Tue Mar 17, 2015 9:46 pm

yes i can share it later (at version 1.0)

at the moment i try to kill last bugs in the sketch

i have a big problem with the wifi connection it is not stable

after x time i can`t reconnect to server

User avatar
chao.zhang
Kindergarten
Kindergarten
Posts: 81
Joined: Thu Jan 22, 2015 9:55 am

Re: Terrarium controled by Linkit ONE

Post by chao.zhang » Thu Apr 02, 2015 5:31 pm

Dear Kevin,

I saw you post this as a recipe on the web.

Now we are giving away Rainbow Cubes, can you send an e-mail to recipe@seeed.cc so that we can discuss more details about this ?

Post Reply