LinkIt ONE SDK for OSX

Moderator: violet

Post Reply
agustin.pelaez
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Thu Nov 06, 2014 12:27 pm

Re: LinkIt ONE SDK for OSX

Post by agustin.pelaez » Fri Apr 17, 2015 5:07 am

**UPDATE**

I was finally able to upload a sketch!

1- I could flash the new firmware by pressing the RST button in the board several times, while clicking once on the green button of the FirmwareUpdater. It's a bit of hit-and-miss but at some point it worked.

2- To upload a sketch select the port "/dev/cu.usbmodem1423" as shown in the pic (I'm not sure why, but the port showed up with the switch of the Linkit to "MS" but then I can still upload sketched when it's set to "UART" mode)

3- To watch the serial monitor, select the other port "/dev/cu.usbmodem1421 (LinkIt ONE)" and then open Arduino's serial console.

Will now try to play with the GPRS modem to connect to http://ubidots.com

sebastian5
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Apr 29, 2015 7:31 pm

Re: LinkIt ONE SDK for OSX

Post by sebastian5 » Sat May 09, 2015 12:30 am

No chance to install that driver.

I use OSX 10.10.3.

I enable Dev Mode (like the readme.txt says).

Then I start the mpkg. It seems to run fine, writes files, etc. but in the end there is always an error message.

"The installation failed.
The installer encountered an error that caused ..."

sebastian5
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Apr 29, 2015 7:31 pm

Re: LinkIt ONE SDK for OSX

Post by sebastian5 » Sun May 10, 2015 4:29 am

Got it to work!

Upload works. You just need to press the reset button on the Linkit after every upload.

I used the alternative cdc acm drivers from here:

http://www.mytracks4mac.info/c/index.ph ... yosemite-2

steven.si
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sat Jul 18, 2015 1:50 am

Re: LinkIt ONE SDK for OSX

Post by steven.si » Sat Jul 18, 2015 1:59 am

Please DO NOT follow the instructions here, as they are outdated. PLEASE follow the instructions on the official MediaTek Labs site: http://labs.mediatek.com/onestart
Last edited by steven.si on Wed Jul 22, 2015 11:52 pm, edited 1 time in total.

sebastian5
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Apr 29, 2015 7:31 pm

Re: LinkIt ONE SDK for OSX

Post by sebastian5 » Mon Jul 20, 2015 6:19 pm

A Link would be nice.

steven.si
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sat Jul 18, 2015 1:50 am

Re: LinkIt ONE SDK for OSX

Post by steven.si » Wed Jul 22, 2015 11:51 pm

The OFFICIAL site for LinkIt ONE SDK for Arduino on Mac OS X is http://labs.mediatek.com/onestart.

Post Reply