NFC Shield 2.0 Compatibility

Moderators: lily.li, violet, salmanfarisvp

Post Reply
dave.corradini
Pre-kindergarten
Pre-kindergarten
Posts: 7
Joined: Tue May 27, 2014 8:11 pm

NFC Shield 2.0 Compatibility

Post by dave.corradini » Tue Jan 13, 2015 9:41 pm

Hi,
I'd like to know if the NFC Shield 2.0 from Seeedstudio is compatible with the Linkit One?
If yes, are there some changes that have to be done, hardware or software?
I tried to connect the two but all I get is "Cannot fint PNXXX board".

Anyone can help?

Thank you!!

Davide

172512376
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Thu Dec 11, 2014 5:14 pm

Re: NFC Shield 2.0 Compatibility

Post by 172512376 » Fri Jan 16, 2015 2:04 pm

Please try to use D9 as SPI_SS, thanks~
You need to change the board as well, please refer to
http://www.seeedstudio.com/wiki/NFC_Shi ... escription

dave.corradini
Pre-kindergarten
Pre-kindergarten
Posts: 7
Joined: Tue May 27, 2014 8:11 pm

Re: NFC Shield 2.0 Compatibility

Post by dave.corradini » Sat Jan 17, 2015 7:45 am

Why? What is the problem on using D10, it has the same specifications as D9.

dave.corradini
Pre-kindergarten
Pre-kindergarten
Posts: 7
Joined: Tue May 27, 2014 8:11 pm

Re: NFC Shield 2.0 Compatibility

Post by dave.corradini » Fri Mar 06, 2015 1:57 am

up!

Again, is it possible to use this shield with the linkit one?!

Thank you

Post Reply