Get Lipo rider pro to charge Ipod or Iphone

Can't find a proper forum to drop the topic, drop here.

Moderators: lily.li, violet

Post Reply
peter_hoenen
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Thu Jun 28, 2012 5:47 am

Get Lipo rider pro to charge Ipod or Iphone

Post by peter_hoenen » Sat Jul 28, 2012 1:19 am

The original design does not a allow the charging of Apple devices because a voltage divider network between B+ and D+ to ground and from B+ and D- to ground is missing.

Solution:

Solder a 75K resistor to B+ and connect the other end to a 50K resistor that goes to ground or B-
The interconnection goes to D+

Repeat the same with another resistor combination of same values for D-

have fun!
Peter

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by deray » Mon Jul 30, 2012 4:28 pm

:) Hello,
Thanks for your sharing , that is cool . I will test it , and put it on the wiki as an example .

Deray

peter_hoenen
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Thu Jun 28, 2012 5:47 am

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by peter_hoenen » Wed Aug 01, 2012 2:59 am

Hi Deray

please have a look at the circuit diagramm of the MintyBoost and implement the same resistor network on the USB output for the LipoRider Pro.

A Lipo protection circuit (over discharge, deep discharge, over current) on the PCB would make the LipoRider even better and a top seller :D :D

Regards
Peter

twan
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sun Sep 16, 2012 11:24 pm
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: 1W Solar Panel 80X100

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by twan » Tue Sep 18, 2012 8:29 am

Hi Peter,

I'm about to upgrade a LipoRider Pro board in order to charge an iPhone.

I wanted to clarify what you meant by B+,B-,D+, and D-.

Can you confirm the following?
For B+ and B-, you mean the + and - for the battery voltage i.e. "+BAT" and "-BAT" on the board.
For D+ and D-, you mean the two central connections on the outgoing USB port.

Is that correct? Thanks for your help!

(And I also agree with your suggestion regarding a protection circuit)

Deray - Will this work with a solar panel of this type?
http://www.seeedstudio.com/depot/1w-sol ... ?cPath=155

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by deray » Tue Sep 25, 2012 3:09 pm

To twan :
yes , all the solar panel we are selling can be used with Lipo rider pro .

Deray

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by deray » Sat Oct 13, 2012 10:13 am


johnmbell
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Tue Nov 20, 2012 5:26 pm

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by johnmbell » Tue Nov 20, 2012 5:51 pm

I'm building one of these to charge my phone while I'm hiking/skiing overnight.

It seems as though Mike & Nancy designed the lipo rider pro with iphone/ipod charging in mind (See Fig. A.) There is no need to solder one resistor to another, just place them to match up with the silk screened lines. So:

R26 = 75K
R25 = 50K
R28 = 75K
R27 = 50K

Will set your device to pull 500mA, whereas:

R26 = 75K
R25 = 50K
R28 = 50K
R27 = 50K

Will let your iDevice pull 1000mA, and charge much faster.

My only piece of constructive feedback for this product would be to upgrade the chip to allow the LiPo battery to charge @ 1000mA (or more) via the mini-USB port, which should really be upgraded to micro-USB (ok, two pieces.) Charging the 6A battery takes ~12 hours, at this point.



Figure A
Image
Last edited by johnmbell on Fri Nov 23, 2012 5:21 pm, edited 2 times in total.

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Get Lipo rider pro to charge Ipod or Iphone

Post by Jacket Chen » Fri Nov 23, 2012 10:50 am

hey ,that's so cool. we can find more interesting things , yet?
Love little, love long.

Post Reply