HELP! Beaglebone Green cannot boot

Moderators: lily.li, violet, salmanfarisvp, seth.welday

Post Reply
charles99.chao
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Tue Nov 20, 2018 8:30 am

HELP! Beaglebone Green cannot boot

Post by charles99.chao » Wed Apr 03, 2019 1:46 pm

Hi,
Can Anyone Help! What should I do?
I tried to control a 4 dc motors 13 sensors setup (4 PWM 8 DO and 13 DI) boot from eMMC without SD card.
After I edited python program for the control but could not save it although I login in with "sudo su".
Then I tried to reboot with usb to pc but then pc can not detect BBG, NO matter using WIN7 or WIN10.
I can not get 192.168.7.2 connected neither by using Ethernet connector.
Now when I plug in usb, LED D1 always ON, D2~D5 ALL ON for seconds then D2 blink as heartbeat, D3 off, D4 blink, D5 ON for a second then off.
And windows did not detect anything.

My basics are:

Code: Select all

debian@beaglebone:~$ sudo /opt/scripts/tools/version.sh
git:/opt/scripts/:[e9bcff232834702c1c810710706ee815d77b080b]
eeprom:[A335BNLTBBG1BBG217084362]
model:[TI_AM335x_BeagleBone_Green]
dogtag:[BeagleBoard.org Debian Image 2018-10-07]
bootloader:[eMMC-(default)]:[/dev/mmcblk1]:[U-Boot 2018.09-00002-g0b54a51eee]:[l     ocation: dd MBR]
kernel:[4.14.71-ti-r80]
nodejs:[v6.14.4]
uboot_overlay_options:[enable_uboot_overlays=1]
uboot_overlay_options:[uboot_overlay_pru=/lib/firmware/AM335X-PRU-RPROC-4-14-TI-     00A0.dtbo]
uboot_overlay_options:[enable_uboot_cape_universal=1]
pkg check: to individually upgrade run: [sudo apt install --only-upgrade <pkg>]
pkg:[bb-cape-overlays]:[4.4.20181120.0-0rcnee0~stretch+20181120]
pkg:[bb-wl18xx-firmware]:[1.20180517-0rcnee0~stretch+20180517]
pkg:[kmod]:[23-2rcnee1~stretch+20171005]
pkg:[librobotcontrol]:[1.0.4-git20181123.0-0rcnee0~stretch+20181124]
pkg:[firmware-ti-connectivity]:[20170823-1rcnee1~stretch+20180328]
groups:[debian : debian adm kmem dialout cdrom floppy audio dip video plugdev us     ers systemd-journal i2c bluetooth netdev cloud9ide gpio pwm eqep admin spi tisdk      weston-launch xenomai]
cmdline:[console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/m     mcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 quiet]
dmesg | grep pinctrl-single
[    1.132112] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
dmesg | grep gpio-of-helper
[    1.144292] gpio-of-helper ocp:cape-universal: ready
END

charles99.chao
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Tue Nov 20, 2018 8:30 am

Re: HELP! Beaglebone Green cannot boot

Post by charles99.chao » Mon Apr 08, 2019 3:38 pm

Hi,
For the record!
I used Ext2Fsd to edit uEnv.txt of SD card and boot BBG from SD card.
And then mount the eMMC block to copy files.
NOW I am good to see what's going on to the BBG for not booting.

Post Reply