I just bought the Raspberry Pi Relay Board v1.0 and I was told that it could output 24 Volts DC

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Thu Jun 20, 2019 6:15 pm

Hi,
I just bought the Raspberry Pi Relay Board v1.0 and I was told that it could output 24 Volts DC .
I need to connect my raspberry pi to a mist maker that takes 24 Volts. So the solution was to use this relay.
My question is how do I specify the output of 24 Volts ?

Thanks

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Fri Jun 21, 2019 9:31 am

Hi there,


The Max output is 30VDC. So it supports 24vdc.   

Thanks

best rgds
Bill


Post Reply