5 inch 720x1280 HDMI IPS LCD Display Dimensions

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

5 inch 720x1280 HDMI IPS LCD Display Dimensions

Post by Anonymous » Wed May 15, 2019 12:49 pm

Hi,

I'm very interested in the 5 inch 720x1280 HDMI IPS LCD Display (SKU:
104990442) for a project I will be doing. One thing I need to know that I
couldn't find on the product description is how deep the screen, including
driver the board, is. The datasheet looks like it only specifies the depth
of the screen itself, not including the I/O board with the connectors. I'm
working in a tight space, so I need to know if the screen will fit. I can
see that the product description says it's 134mm wide x 84mm tall. I just
need to know the depth dimension before I can make a decision.

Thanks,

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Wed May 15, 2019 4:38 pm

Hi, 

The Screen is around 9mm and the driver board is 15mm. Total is 24cm. Thanks

Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Wed May 15, 2019 11:55 pm

Great, thanks! Can I also ask the same question about the 7" version
(SKU: 104990443)? I might be able to squeeze the bigger height and width if
it's a similar depth.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Thu May 16, 2019 9:21 am

Hi 

It is the same height as 5 inch.Thanks

Post Reply