Temp & Humidity Sensor Pro

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
nabosakproductions
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Wed Feb 13, 2019 3:50 am

Temp & Humidity Sensor Pro

Post by nabosakproductions » Wed Feb 13, 2019 4:13 am

Hello,

I have had Raspberry Pi in the past and enjoyed them. But I am still not great at understanding how to work with the GrovePi+. I currently have a Raspberry Pi 3 Model B with a GrovePi+ and a Temp and Humidity Sensor Pro.

I followed the setup instructions:
http://wiki.seeedstudio.com/Grove-Tempe ... spberry-pi

When I run:
sudo nano grove_dht_pro.py (in the terminal)

I get a GNU nano 2.7.4 File: grove_dht_pro.py

And it is just a blank black screen (Also says New File at the bottom)
The very first time had licensing text and links to the above weblink I have provided and this forum.

The code shown in the next step:

import grovepi
import math

ect...

Did not show up in the terminal like I had expected it.
When I tried running this code in the PythonIDLE it said "No module named 'grovepi'"

Am I supposed to be running this code in a different enviroment? I am not sure which one. It looked like python code to me.

Please help I would like to start gather data from the sensor

Thank you,
Nicholas

bill.yu
Elementary-5
Elementary-5
Posts: 597
Joined: Mon Apr 02, 2018 11:05 am

Re: Temp & Humidity Sensor Pro

Post by bill.yu » Mon Mar 04, 2019 5:43 pm

HI Nicholas,

1. which folder do you locate when you run "sudo nano grove_dht_pro.py"?
the python file is located at ~/GrovePi/Software/Python. please do make sure you go to the folder first before editing the grove_dht_pro.py.

2. for the "No module named 'grovepi'", please follow https://www.dexterindustries.com/GroveP ... -software/ to configure the development environment. you can follow the Quickstart Directions as below.

In the command line, type the following commands:

sudo curl -kL dexterindustries.com/update_grovepi | bash
sudo reboot

After your Raspberry Pi reboots, the GrovePi is ready to use!

We hope it can help. thanks.

Post Reply