CanBus v1.2 message delay and HEX structure

Ardiuno Compatible shields

Moderators: lily.li, violet

Post Reply
hornetmech21
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Mon Jan 21, 2019 10:43 pm

CanBus v1.2 message delay and HEX structure

Post by hornetmech21 » Wed Jan 23, 2019 12:12 pm

Hi everyone,
The past few weeks have gone really well using the canbus shield v1.2 for pulling a can dump from both my pontiac and my friends FRS. I was even able to broadcast RPM back to the pontiac and have it change the tach with the engine off.

Currently, I have the electronic steering system out of the FRS on a test bench in my living room, and need to broadcast (18) Can ID's over the network. After a few weeks of recording and translating the Id's from the car and rebroadcasting them, I haven't had any success getting the test rig to respond.

I have 2 questions that I havn't been able to find answers for:
1) Can I just use CAN.sendMsgBuf one after another or do I need a delay after it? If I do use a delay, does it interfere with transmitting at the right times on the 500kbps bus?

2) I am structuring the message "buff" for each ID as I recorded it. Should the buff be structured as I have it in HEX? or should I input decimal and the shield takes care of translating? MY code is below for anyone that might see something that I'm doing wrong. Thanks for the help.

Code: Select all

// demo: CAN-BUS Shield, send data
// loovee@seeed.cc

#include <mcp_can.h>
#include <SPI.h>

// the cs pin of the version after v1.1 is default to D9
// v0.9b and v1.0 is default D10
const int SPI_CS_PIN = 9;

MCP_CAN CAN(SPI_CS_PIN);

unsigned char msg144[8] = {0xC0, 0x0, 0x71, 0x8A, 0x44, 0xA4, 0xA0, 0x0};// 0x140 70mph C0 0 71  8A  44  A4  A0  0
unsigned char msg360[8] = {0x96, 0x7, 0x87, 0x80, 0x37, 0x80, 0x1, 0x0};// 0x360 70mph: 96  7 87  80  37  80  1 0
unsigned char msg282[8] = {0xB0, 0xB1, 0x8A, 0x64, 0x64, 0x0, 0x20, 0x0};//282 70MPH :     B0  B1  8A  64  64  0 20  0
unsigned char msg142[8] = {0x5B, 0x26, 0x8, 0x0, 0x0, 0x0, 0x0, 0x0};//0X142 70MPH       5B  26  8 0 0 0 0 0
unsigned char msg361[8] = {0x5, 0x29, 0x0, 0xD8, 0xD, 0xB0, 0x85, 0x79}; //5 29  0 D8  D B0  85  79
unsigned char msg152[8] = {0xF0, 0xE4, 0x0, 0x0, 0x0, 0x2, 0x0, 0x4C};
unsigned char msg372[8] = {0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0};// 0X372   0 0 0 0 0 0 0 0
unsigned char msg4DD[8] = {0x1E, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0}; ///1E  0 0 0 0 0 0 0  (159661)
unsigned char msg4C1[8] = {0x1, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0};//1  0 0 0 0 0 0 0
int dT = 0;//easy to change the delay between sending mesages


void setup() {
  Serial.begin(115200);

  while (CAN_OK != CAN.begin(CAN_500KBPS))              // init can bus : baudrate = 500k
  {
    Serial.println("CAN BUS Shield init fail");
    Serial.println(" Init CAN BUS Shield again");
    delay(100);
  }
  Serial.println("CAN BUS Shield init ok!");
  // Serial.println(msg18[2]);
}

void loop() {
  CAN.sendMsgBuf(0x144, 0, 8, msg144); delay(dT);

  CAN.sendMsgBuf(0x360, 0, 8, msg360); delay(dT);

  CAN.sendMsgBuf(0x282, 0, 8, msg282); delay(dT);

  CAN.sendMsgBuf(0x142, 0, 8, msg142); delay(dT);

  CAN.sendMsgBuf(0x361, 0, 8, msg361); delay(dT);

  CAN.sendMsgBuf(0x152, 0, 8, msg152); delay(dT);

  CAN.sendMsgBuf(0x372, 0, 8, msg372); delay(dT);

  CAN.sendMsgBuf(0x4DD, 0, 8, msg4DD); delay(dT);

  CAN.sendMsgBuf(0x4C1, 0, 8, msg4C1); delay(dT);

}

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 85
Joined: Wed Jan 30, 2019 11:51 am

Re: CanBus v1.2 message delay and HEX structure

Post by bestlux » Wed Jan 30, 2019 6:09 pm

1)Baud rate is an attribute of signals, and delay determines the gap between each time signal transmitted, which is independent of each other.
2)Data type is basic knowledge of Computer Science. If you are interested in it, you can study the relevant books of C and C++.

hornetmech21
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Mon Jan 21, 2019 10:43 pm

Re: CanBus v1.2 message delay and HEX structure

Post by hornetmech21 » Thu Jan 31, 2019 12:43 pm

LOL Bestlux. so you joined today, just to insult my lack of knowledge? trolls everywhere smh.

I'm hoping someone else has some thoughts other than "go get a degree in computer science"

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 85
Joined: Wed Jan 30, 2019 11:51 am

Re: CanBus v1.2 message delay and HEX structure

Post by bestlux » Thu Jan 31, 2019 2:38 pm

Hello,I'm sorry for being some kind of impolite because of my poor language skill. I'm a novice of English, surfing in the forum for improving my communication skill. And after reading your post, I think you have successfully completed the experiment successfully, but still have some questions, that are just for curiosity.
Your question is a very basic knowledge of programming, and you can find your answer easily through Wiki or any programming tutorial.
Please refer to this link:
https://en.wikipedia.org/wiki/Data_type
Specifically, Hex and Decimal are just different representations of the same values, and they are eventually translated into the same 0 and 1 in memory by the compiler.
For example, following two line of code does the same thing.

Code: Select all

unsigned char msg[8] = {0x5, 0x29, 0x0, 0xD8, 0xD, 0xB0, 0x85, 0x79}; 

Code: Select all

unsigned char msg[8] = {5, 41, 0, 216, 13, 176, 133, 121};
They all create a section of memory with the same content as:

I hope my answer will help you.
Best regards,

User avatar
designnotes.com
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Mon Jan 28, 2019 11:08 pm
Location: Philadelphia, PA
Contact:

Re: CanBus v1.2 message delay and HEX structure

Post by designnotes.com » Sat Feb 09, 2019 11:02 pm

hornetmech21 wrote:
Wed Jan 23, 2019 12:12 pm
Hi everyone,
The past few weeks have gone really well using the canbus shield v1.2 for pulling a can dump from both my pontiac and my friends FRS. I was even able to broadcast RPM back to the pontiac and have it change the tach with the engine off.

Currently, I have the electronic steering system out of the FRS on a test bench in my living room, and need to broadcast (18) Can ID's over the network. After a few weeks of recording and translating the Id's from the car and rebroadcasting them, I haven't had any success getting the test rig to respond.

I have 2 questions that I havn't been able to find answers for:
1) Can I just use CAN.sendMsgBuf one after another or do I need a delay after it? If I do use a delay, does it interfere with transmitting at the right times on the 500kbps bus?

2) I am structuring the message "buff" for each ID as I recorded it. Should the buff be structured as I have it in HEX? or should I input decimal and the shield takes care of translating? MY code is below for anyone that might see something that I'm doing wrong. Thanks for the help.

Code: Select all

// demo: CAN-BUS Shield, send data
// loovee@seeed.cc

#include <mcp_can.h>
#include <SPI.h>

// the cs pin of the version after v1.1 is default to D9
// v0.9b and v1.0 is default D10
const int SPI_CS_PIN = 9;

MCP_CAN CAN(SPI_CS_PIN);

unsigned char msg144[8] = {0xC0, 0x0, 0x71, 0x8A, 0x44, 0xA4, 0xA0, 0x0};// 0x140 70mph C0 0 71  8A  44  A4  A0  0
unsigned char msg360[8] = {0x96, 0x7, 0x87, 0x80, 0x37, 0x80, 0x1, 0x0};// 0x360 70mph: 96  7 87  80  37  80  1 0
unsigned char msg282[8] = {0xB0, 0xB1, 0x8A, 0x64, 0x64, 0x0, 0x20, 0x0};//282 70MPH :     B0  B1  8A  64  64  0 20  0
unsigned char msg142[8] = {0x5B, 0x26, 0x8, 0x0, 0x0, 0x0, 0x0, 0x0};//0X142 70MPH       5B  26  8 0 0 0 0 0
unsigned char msg361[8] = {0x5, 0x29, 0x0, 0xD8, 0xD, 0xB0, 0x85, 0x79}; //5 29  0 D8  D B0  85  79
unsigned char msg152[8] = {0xF0, 0xE4, 0x0, 0x0, 0x0, 0x2, 0x0, 0x4C};
unsigned char msg372[8] = {0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0};// 0X372   0 0 0 0 0 0 0 0
unsigned char msg4DD[8] = {0x1E, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0}; ///1E  0 0 0 0 0 0 0  (159661)
unsigned char msg4C1[8] = {0x1, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0};//1  0 0 0 0 0 0 0
int dT = 0;//easy to change the delay between sending mesages


void setup() {
  Serial.begin(115200);

  while (CAN_OK != CAN.begin(CAN_500KBPS))              // init can bus : baudrate = 500k
  {
    Serial.println("CAN BUS Shield init fail");
    Serial.println(" Init CAN BUS Shield again");
    delay(100);
  }
  Serial.println("CAN BUS Shield init ok!");
  // Serial.println(msg18[2]);
}

void loop() {
  CAN.sendMsgBuf(0x144, 0, 8, msg144); delay(dT);

  CAN.sendMsgBuf(0x360, 0, 8, msg360); delay(dT);

  CAN.sendMsgBuf(0x282, 0, 8, msg282); delay(dT);

  CAN.sendMsgBuf(0x142, 0, 8, msg142); delay(dT);

  CAN.sendMsgBuf(0x361, 0, 8, msg361); delay(dT);

  CAN.sendMsgBuf(0x152, 0, 8, msg152); delay(dT);

  CAN.sendMsgBuf(0x372, 0, 8, msg372); delay(dT);

  CAN.sendMsgBuf(0x4DD, 0, 8, msg4DD); delay(dT);

  CAN.sendMsgBuf(0x4C1, 0, 8, msg4C1); delay(dT);

}
I have 2 questions that I havn't been able to find answers for:
1) Can I just use CAN.sendMsgBuf one after another or do I need a delay after it? If I do use a delay, does it interfere with transmitting at the right times on the 500kbps bus?

It is better to add delay between each message see the code for sendMsgBuf. It returns a byte CAN_OK if messages sends successfully.

Code: Select all


/*********************************************************************************************************
** Function name:           sendMsgBuf
** Descriptions:            Send message by using buffer read as free from CANINTF status
**                          Status has to be read with readRxTxStatus and filtered with checkClearTxStatus
*********************************************************************************************************/
byte MCP_CAN::sendMsgBuf(byte status, unsigned long id, byte ext, byte rtrBit, byte len, volatile const byte *buf)
{
  byte txbuf_n=statusToTxSidh(status);

  if ( txbuf_n==0 ) return CAN_FAILTX; // Invalid status

  mcp2515_modifyRegister(MCP_CANINTF, status, 0);  // Clear interrupt flag
  mcp2515_write_canMsg(txbuf_n, id, ext, rtrBit, len, buf);

  return CAN_OK;
}
2) I am structuring the message "buff" for each ID as I recorded it. Should the buff be structured as I have it in HEX? or should I input decimal and the shield takes care of translating? MY code is below for anyone that might see something that I'm doing wrong. Thanks for the help.
I don't get your this query. I hope the first one will help you.

Post Reply