GPRS shield turns off on incoming call

Ardiuno Compatible shields

Moderators: lily.li, violet

Post Reply
tuyenhq1994
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Sep 06, 2018 4:39 pm

GPRS shield turns off on incoming call

Post by tuyenhq1994 » Tue Jan 08, 2019 11:26 am

Hello!
I'm using GPRS shield v1.2 mounted to Arduino Mega 1280.
I've loaded the test program (to use HyperTerminal for sending commands from PC) to Arduino and tested it.
It works fine (I've sent "AT" and received "OK"). Status and Netlight leds are on. Netlight blinks 64ms On/3000ms Off.

After that I've tried to call to phone number of SIM card installed to GPRS shield.
In this case - GPRS shield turns off immediately. Status and Netlight leds switches off.
The SIM card I use is from my personal phone and it works fine. Arduino Mega connected to PC through the USB cable and powers from it.

Could you please tell me what could be the root of problem?

[UPD]
Problem solved. The cause is bad powering via USB cable. Arduino should be powered by adapter

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 85
Joined: Wed Jan 30, 2019 11:51 am

Re: GPRS shield turns off on incoming call

Post by bestlux » Thu Jan 31, 2019 11:03 am

Hello,
Sounds that you have already solved your problem, using USB for powering is a common mistake, I even burn my USB interface when I am a novice.
Thank you for your support.
Good luck!

Post Reply