Page 1 of 1

SeeedMotorShieldV2-master.zip

Posted: Sat Apr 02, 2016 3:16 am
by schij12
Guru's

First time member, first time post.

For some reason I can't run both motors at the same time with the V2.2 motor shield.

I followed the code instructions but they do not both fire off. Sample code below.

void loop()
{
motor.speed(0, 100);
motor.speed(1, 100);

----
The only way I can get the second channel to work if I do this:

void setup()
{
// initialize
motor.begin();
digitalWrite(9, HIGH);
digitalWrite(10, HIGH);
}

Any help would be great.

Thank you.

Joey

Re: SeeedMotorShieldV2-master.zip

Posted: Mon Apr 04, 2016 1:50 pm
by kavi
Hi Joey,

Please use the library in the following link.

Thanks and Regards