CAN-BUS Shield V1.2 and OBDII Library

Hello everyone. In CAN-BUS Shield wiki page I read:

“With an OBD-II converter cable added on and the OBD-II library imported, you are ready to build an onboard diagnostic device or data logger.”

Ok…I have the cable and the shield, but where is the OBD-II library?

Thanks

Andrea

Hi, I am sorry there’s no obd library, but a simple demo, please refer to github.com/Seeed-Studio/CANBUS_ … BD_RECIPLE

Thanks.

Check out this:
https://www.libelium.com/api/waspmote/df/d8b/WaspCAN_8h_source.html
This is the only library I have found. It is limited though. I would like to start working on this, but I’m not sure if there is the demand for it.