Page 1 of 1

TFT Touch Shield V1.0 with Leonardo?

Posted: Wed Feb 11, 2015 11:12 am
by xxobsoletexx
Hi everyone,

I bought a Touch Shield from RadioShack for a steal of $15 this afternoon, and it's been fun to play with. After playing with it on my Uno, I decided I wanted to use it with my Leonardo as a small touch-screen keyboard.

It didn't work, and I found mention on Adafruit's site about it not being compatible with the Leonardo.

I was wondering, why isn't it compatible? Is there something I can do to make it work with the Leonardo, or is it impossible?

Re: TFT Touch Shield V1.0 with Leonardo?

Posted: Fri Feb 13, 2015 3:25 pm
by kavi
Hello,

Could you please check if the example code mentioned in http://www.seeedstudio.com/wiki/2.8''_T ... hield_V1.0 . It looks like the necessary pin re-mapping for Leonardo is mentioned in that code :

Code: Select all

#elif defined(__AVR_ATmega32U4__) // leonardo
#define YP A2   // must be an analog pin, use "An" notation!
#define XM A1   // must be an analog pin, use "An" notation!
#define YM 18   // can be a digital pin, this is A0
#define XP 21   // can be a digital pin, this is A3 
Thanks

Re: TFT Touch Shield V1.0 with Leonardo?

Posted: Fri Mar 06, 2015 1:32 am
by pjkim00
Pick up a Touch Shield v1 at Radio Shack and got it to work with a Leonardo. It was a bit more involved than changing just the resistive pins (i.e. XM, XP, YM, YP). The pin mappings from D2 through D9 to the microcontroller pins is very different. Here are the pin mappings for Uno, Mega, and Leonardo:

Code: Select all

Pin   d9   d8   d7   d6   d5   d4   d3   d2
Uno   PB1  PB0  PD7  PD6  PD5  PD4  PD3  PD2
Mega  PH6  PH5  PH4  PH3  PE3  pg5  PE5  PE4
Leon  PB5  PB4  PE6  PD7  PC6  PD4  PD0  PD1
The code changes to TFT.cpp are shown below. The first set of changes are at the start of the file and the second at the end.

Change TFT::pushData and TFT::getData as follows:

Code: Select all

void TFT::pushData(unsigned char data)
{
    all_pin_low();
#ifdef ARDUINO_AVR_LEONARDO
    PORTD |= ((data<<1) & (0x02));
    PORTD |= ((data>>1) & (0x01));
    PORTD |= ((data<<2) & (0x10));	
    PORTC |= ((data<<3) & (0x40));	
    PORTD |= ((data<<3) & (0x80));	
    PORTE |= ((data<<1) & (0x40));
    PORTB |= ((data>>2) & (0x30));	
#else ifdef SEEEDUINO
    PORTD |= (data<<2);
    PORTB |= (data>>6);
#endif

#ifdef MEGA
    PORTE |= ((data<<4) & (0x30));
    PORTG |= ((data<<3) & (0x20));
    PORTE |= ((data & 0x08));
    PORTH |= ((data>>1) & (0x78));
#endif

#ifdef MAPLE
#endif
}

unsigned char TFT::getData(void)
{
    unsigned char data=0;
    delay(1);
#ifdef ARDUINO_AVR_LEONARDO
	data |= ((PIND&0x02)>>1);	//PD1
	data |= ((PIND&0x01)<<1);	//PD0
	data |= ((PIND&0x10)>>2);	//PD4
	data |= ((PINC&0x40)>>3);	//PC6
	data |= ((PIND&0x80)>>3);	//PD7
	data |= ((PINE&0x40)>>1);	//PE6
	data |= ((PINB&0x30)<<2);	//PB4,5
#else ifdef SEEEDUINO
    data |= ((PIND&0xfc)>>2);
    data |= ((PINB&0x03)<<6);
#endif

    return data;
}
And at the end, change the following

Code: Select all

void TFT::all_pin_input(void)
{

#ifdef ARDUINO_AVR_LEONARDO
	DDRD &=~ 0x93;
	DDRC &=~ 0x40;
	DDRE &=~ 0x40;
	DDRB &=~ 0x30;
#else ifdef SEEEDUINO
    DDRD &=~ 0xfc;
    DDRB &=~ 0x03;
#endif
#ifdef MEGA
    DDRE &=~ 0x38;
    DDRG &=~ 0x20;
    DDRH &=~ 0x78;
#endif

#ifdef MAPLE

#endif

}

void TFT::all_pin_output(void)
{
#ifdef ARDUINO_AVR_LEONARDO
	DDRD |= 0x93;
	DDRC |= 0x40;
	DDRE |= 0x40;
	DDRB |= 0x30;
#else ifdef SEEEDUINO
    DDRD |= 0xfc;
    DDRB |= 0x03;
#endif


#ifdef MEGA
    DDRE |= 0x38;
    DDRG |= 0x20;
    DDRH |= 0x78;
#endif

#ifdef MAPLE

#endif
}

void TFT::all_pin_low(void)
{

#ifdef ARDUINO_AVR_LEONARDO
	PORTD &=~ 0x93;
	PORTC &=~ 0x40;
	PORTE &=~ 0x40;
	PORTB &=~ 0x30;
#else ifdef SEEEDUINO
    PORTD &=~ 0xfc;
    PORTB &=~ 0x03;
#endif
#ifdef MEGA
    PORTE &=~ 0x38;
    PORTG &=~ 0x20;
    PORTH &=~ 0x78;
#endif

#ifdef MAPLE

#endif
}

TFT Tft=TFT();
And lastly, make changes in TFT.h file. Replace line that starts with #ifdef SEEEDUINO with

Code: Select all

#ifdef ARDUINO_AVR_LEONARDO

//======================================== PB6
#define DDR_CS      DDRB
#define PORT_CS     PORTB
#define CS_BIT      0x40
#define CS_OUTPUT   {DDR_CS|=CS_BIT;}
#define CS_HIGH     {PORT_CS|=CS_BIT;}
#define CS_LOW      {PORT_CS&=~CS_BIT;}

//----------------------------------------- PB7

#define DDR_RS      DDRB
#define PORT_RS     PORTB
#define RS_BIT      0x80
#define RS_OUTPUT   {DDR_RS|=RS_BIT;}
#define RS_HIGH     {PORT_RS|=RS_BIT;}
#define RS_LOW      {PORT_RS&=~RS_BIT;}

//-----------------------------------------  PD6

#define DDR_WR      DDRD
#define PORT_WR     PORTD
#define WR_BIT      0x40
#define WR_OUTPUT   {DDR_WR|=WR_BIT;}
#define WR_HIGH     {PORT_WR|=WR_BIT;}
#define WR_LOW      {PORT_WR&=~WR_BIT;}
#define WR_RISING   {PORT_WR|=WR_BIT;PORT_WR&=~WR_BIT;}

//----------------------------------------- PC7

#define DDR_RD      DDRC
#define PORT_RD     PORTC
#define RD_BIT      0x80
#define RD_OUTPUT   {DDR_RD|=RD_BIT;}
#define RD_HIGH     {PORT_RD|=RD_BIT;}
#define RD_LOW      {PORT_RD&=~RD_BIT;}
#define RD_RISING   {PORT_RD|=RD_BIT;PORT_RD&=~RD_BIT;}
//========================================

#else ifdef SEEEDUINO
If the code maintainer could incorporate these changes, that would be great.