TFT V2.0 SHIELD , Pinout NAMES .

Ardiuno Compatible shields

Moderators: lily.li, violet

Post Reply
yam1000r1
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Wed Jan 15, 2014 8:47 am

TFT V2.0 SHIELD , Pinout NAMES .

Post by yam1000r1 » Wed Jan 15, 2014 11:08 am

Hy Seeed Studio Community ,

I bought a 2.8" TFT LCD on an SeeedStudio Shield ( V2.0 / ILI9341 ), and would like to know the reference PIN for this one .
Image
I found , after couple of hours these pin names , but I don't Find any information about Pin 0,1,2,3,8 and 9 .
And why are AREF and Vin Connected ? Are they used by the LCD ? ( I don't see if they are connected on any signal on the PCB so I ask :) )

Is there anybody could Help me to find them ?

Here What I found :

Code: Select all

Pin           =>     Description
=====================
4             =>    TF_CS, SD card select input pin ( testing if card present or not )
5             =>    TFT_CS, TFT chip select input pin
6             =>    TFT_D/C, TFT Data/Command control pin
7             =>    BACKLIGHT, TFT backlight control pin
10            =>   SPI chip select
11            =>   SPI data pin
12            =>   SPI data pin
13            =>   SPI serial clock pin
A0            => Touch Screen Y- input pin.
A1            => Touch Screen X- input pin.
A2            => Touch Screen Y+ input pin.
A3            => Touch Screen X+ input pin.
Thanks in advance .

op2op2op2
Alpha User
Posts: 8
Joined: Fri Dec 05, 2014 5:58 pm

Re: TFT V2.0 SHIELD , Pinout NAMES .

Post by op2op2op2 » Tue Dec 09, 2014 5:38 pm

I want to know them also.

PLease

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: TFT V2.0 SHIELD , Pinout NAMES .

Post by kavi » Tue Dec 09, 2014 8:16 pm

Thank you for purchasing the TFT Shield. Have you seen the EAGLE schematic and board files mentioned in Wiki->TFT Touch Shield v2.0

Let me know if you need any other clarification. Thanks

op2op2op2
Alpha User
Posts: 8
Joined: Fri Dec 05, 2014 5:58 pm

Re: TFT V2.0 SHIELD , Pinout NAMES .

Post by op2op2op2 » Tue Dec 09, 2014 8:40 pm

Have you got a PDF of the schema ?

And also, I need a "fake shield" in order to use other arduino pins ? I mean, seeing potos i doubt that I could put athing in the unused arduino pins, couldn't I ?

Best regards,

viswa
Staff
Staff
Posts: 168
Joined: Tue Jan 25, 2011 11:16 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Seeeduino Film,Motion Frame,UartSbee

Re: TFT V2.0 SHIELD , Pinout NAMES .

Post by viswa » Wed Dec 10, 2014 4:06 pm

Hi,

I have uploaded the PDF schematic to wiki. Please check.

TFT Shiled must be the top most shield and you could use Base Shield V2 to access pins not used by TFT.

Thanks

dmarabell
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Tue Dec 30, 2014 11:58 am

Re: TFT V2.0 SHIELD , Pinout NAMES, partlist

Post by dmarabell » Tue Dec 30, 2014 12:03 pm

Where can I find the manufacturers part list for the TFT V2.0 Shield ?

Thanks

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: TFT V2.0 SHIELD , Pinout NAMES .

Post by kavi » Thu Feb 05, 2015 12:36 pm

Hi,
We do not have a separate manufacturers part list .
You could generate a BOM from Eagle CAD files.
Thanks

Post Reply