Why does TFT Touchshield 2.0 need ICSP pins?

Ardiuno Compatible shields

Moderator: violet

Post Reply
nekbet
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Apr 05, 2013 3:48 am

Why does TFT Touchshield 2.0 need ICSP pins?

Post by nekbet » Fri Apr 05, 2013 3:50 am

per the wiki,
http://www.seeedstudio.com/wiki/2.8%27% ... hield_v2.0

The shield is using D10,D11,D12,D13 for the SPI interface.

Why does it need the 6 ICSP connector pins hooked up as well?

I need to put a shield in between the ardo and the screen to do some gyro work.. My go-between shield doesnt have the ICSP passed thru...

thanks,
Mike

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Why does TFT Touchshield 2.0 need ICSP pins?

Post by Jacket Chen » Tue Apr 09, 2013 7:21 pm

Hi, our TFT shield v2 is designed with Arduino or Seeeduino, and the Arduino or Seeeduino has a ICSP port, so our TFT can plug on Arduino directly, it is convenient. And our new version of shields have the same style(with a ICSP port and the same size).And if you just need a ISP port, you can use those pins only via jumprer wire except other two pins(VCC and GND).

And you can refer to schematic of TFT to find those corresponding pins(SPI) on the TFT.
Love little, love long.

Post Reply