Bluetooth Shield on Arduino due

Hi, is the bluetooth shield compatible with arduino due?

The hardware of due are different from Arduino,if you want do that,you may need use Arduino IDE 1.5,and modify some libraries. So,bluetooth shield is not compatible with due directly.

hi, as the bluetooth shield communicate with MCU board(Uno or Due) by uart. so, you just need to use the UART port to receive or sent message via the Bluetooth. the Bluetooth is compatible with Uno to Due by Hardware. but note that you need to set the serial port in Due.