NFC Shield v 2.1 + NFC Antenna

Hi all,



I’m working with NFC shield, but I must to change the antenna’s shape.

I would like to know the following antenna’s parameters:

  • L value at 13.56 MHz
  • Q @13.56 MHz



    I saw that the antenna dimension is 28mm X 30.5mm.



    I would like to know conductor parameters:

    • Width of tracks in mm

    • Spacing between turns in mm

    • Thickness of the conductor in µm





    Thank you

    Manuel

Hi,

Do you want to use an external antenna for NFC? if not can you please more specific?

Yes, I do. I need to change antenna’s shape, so I would like to know some information about the initial Antenna.

Can you help me?



Thank you

Manuel

Information about this antenna right?





Yes, right!



May you send me more informations?



Thanks

Manuel

Hi,



Currently, the design files are not available, but I can provide you design guide for the exact NFC 13.56MHZ ANTENNA . Please let me know if it helps you.