need information about solar charger shield V2.2

Ardiuno Compatible shields

Moderators: lily.li, violet

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

need information about solar charger shield V2.2

Post by Anonymous » Fri Mar 22, 2019 5:19 am

Hi,

Few weeks ago I purchased a Solar Charger Shield V2.2. Could you give
the exacte name of the type of connector used to connect solar pannel
and battery ?

Thank you very much.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Fri Mar 22, 2019 9:13 am

Hi there,


ricardo.herrero
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Mon Sep 30, 2019 6:38 pm

Re: need information about solar charger shield V2.2

Post by ricardo.herrero » Mon Sep 30, 2019 7:24 pm

Hello,

Thanks for the info, I have seen this answer and I will buy the cables, but I also need the connector. I have seen both 2.00mm and 2.54mm. I have bought solar charger v2.2 11/19/2014, which one is valid for me? From the wikipedia we can see the type of connector, which one do I choose?

Thanks for the help,
Ricardo

ricardo.herrero
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Mon Sep 30, 2019 6:38 pm

Re: need information about solar charger shield V2.2

Post by ricardo.herrero » Wed Oct 02, 2019 2:26 pm

I have seen three different connectors but I can´t decide which one is the proper one:
JST PH 2 pin
JST XH 2 pin
JST XHP-2

Which should I choose? This is info that should come with the solar charger v2.2 shield.

Thanks for the help!
Ricardo

595355940
Kindergarten
Kindergarten
Posts: 75
Joined: Tue Oct 23, 2018 5:33 pm

Re: need information about solar charger shield V2.2

Post by 595355940 » Thu Oct 24, 2019 2:11 pm


Post Reply