Arduino R3 UNO + 1.2 CAN BUS, stuck at init, HELP

Ardiuno Compatible shields

Moderators: lily.li, violet

Post Reply
admire123
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Fri Feb 01, 2019 7:05 am

Arduino R3 UNO + 1.2 CAN BUS, stuck at init, HELP

Post by admire123 » Fri Feb 01, 2019 7:19 am

i downloaded the CAN BUS library from https://github.com/Seeed-Studio/CAN_BUS_Shield
running the example "receive_check"

my hardware is
Arduino R3 UNO x 2
Arduino Mega2560 x 1
CAN BUS Shield V1.2 10/23/2014 by Seeed Studio x 2
(i just stack them together)

I tried both
const int SPI_CS_PIN = 9;
const int SPI_CS_PIN = 10;
and changed
#define MCPDEBUG (1)

but after uploaded the program, the serial output

Enter setting mode fail
CAN BUS Shield init fail
Init CAN BUS Shield again
Enter setting mode fail
CAN BUS Shield init fail
Init CAN BUS Shield again
Enter setting mode fail
CAN BUS Shield init fail
Init CAN BUS Shield again

ONLY POWER red LED light up on the shield, other LEDs not lighting up.

(tried power with 12V DC
or USB-serial cable)
(tried solder the CS from 9 to 10 at the back)
(tried 2 different 1.2 CAN BUS SHIELD)
(tried 2 different UNO R3)
(tried Mega2560)
(tried different library , e.g. coryjfowler's)

The result is same, stucking at CAN init, always FAIL

I struggled for 48 hours already, anyone could help and knows what's wrong??

Thanks.

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 85
Joined: Wed Jan 30, 2019 11:51 am

Re: Arduino R3 UNO + 1.2 CAN BUS, stuck at init, HELP

Post by bestlux » Fri Feb 01, 2019 4:00 pm

Hello,
Could you please show me how you connect both boards? Thx
Here is the right method to connect them.
Make sure you have plugged those pins into the position.
Image
If it still does not work, there might be some problem with hardware.
But you have tried two boards; It is little possibility they are all broken. Is your wire all right ?You can test them with a multimeter.
Good luck!

admire123
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Fri Feb 01, 2019 7:05 am

Re: Arduino R3 UNO + 1.2 CAN BUS, stuck at init, HELP

Post by admire123 » Sat Feb 02, 2019 5:52 pm

20190202174954.jpg
20190202174954.jpg (193.65 KiB) Viewed 1110 times
The attachment 20190202174954.jpg is no longer available
My connection is the same as your picture, i tried to use multimeter to test the pins connection, they are connected...guess i got broken shields from a damaged batch boards....

Post Reply