MP3 player 2 with ESP32?

Ardiuno Compatible shields

Moderator: violet

Post Reply
treii28619
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Apr 18, 2018 12:14 am

MP3 player 2 with ESP32?

Post by treii28619 » Thu Oct 11, 2018 10:47 pm

Has anyone had any luck getting the mp3 player v2 to work with ESP32? I tried using it first with SoftSerialESP32, then by using one of the two additional hardware serials and it keeps crashing and restarting no matter what I try to do. I haven't had the opportunity yet to nit-pick the docs or code to try to re-write it more ESP32 friendly or potentially as an object package, and I need to do some checking this afternoon on my Uno with the default sketch to make sure the player I just received is in fact working.
But I figured I'd at least check to see if anyone has used it with an ESP32 because my project is building on a Wemos D1 Mini32 pro

User avatar
bestlux
Pre-kindergarten
Pre-kindergarten
Posts: 28
Joined: Wed Jan 30, 2019 11:51 am

Re: MP3 player 2 with ESP32?

Post by bestlux » Thu Jan 31, 2019 11:34 am

Hello,
You need to change the pin number definition in the code first before you compile the example code.
The pin definitions of esp32 are different from those of Arduino boards. Here is their 1-to-1 relationship.
Image

Post Reply