After my bluetooth bee connect to PC,how can I keep connect?

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
georrge
Pre-kindergarten
Pre-kindergarten
Posts: 15
Joined: Sat May 08, 2010 3:27 pm

After my bluetooth bee connect to PC,how can I keep connect?

Post by georrge » Thu Jul 08, 2010 5:00 pm

I have connected my bluetooth to my PC,but how can I upload my arduino program to board? If I keep bluetooth and shield on arduino board,it can not upload. So, I disassambel bluetooth and shield from arduino board,then it can upload program to arduino board,but it lost connection between bluetooth bee and PC. If I use terminal program to start connect again,it can not do,because arduino board is not empty anymore.

Icing
Elementary-1
Elementary-1
Posts: 140
Joined: Wed Oct 21, 2009 10:39 pm

Re: After my bluetooth bee connect to PC,how can I keep connect?

Post by Icing » Fri Jul 09, 2010 1:28 pm

Hi georrge,

Try to use the command \r\n+STAUTO=1\r\n which will make Bluetooth auto-connect the last paired device on power.

Regards,

-Icing

Post Reply