GPRSbee rev.6

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
vstamos
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Wed Aug 26, 2015 9:22 pm

GPRSbee rev.6

Post by vstamos » Tue Dec 15, 2015 4:46 am

Dear All,

Being new I would like some help.
Using GPRSbee rev.6 on a Sodaq Mbili board. I would like to send data over SMS using 2 different modes:
1: I would like to call the GPRSbee, the GPRSbee to reject my call, read the sensors and reply with an SMS with the reading.
2: Use the RTC, open 1,2,3 etc times a day ( used defined) read the sensors and send SMS.

The first problem which occurred is which commands to use with the GPRSbee rev.6 .
I have done it using sim900 and arduino Uno as follows :

#include "SIM900.h"
#include <SoftwareSerial.h>
#include "call.h"
#include <DHT.h>
#include "sms.h"

SMSGSM sms;
#define DHTPIN 7
#define DHTTYPE DHT22

CallGSM call;
boolean started=false;
char sms_text[160];

DHT dht(DHTPIN, DHTTYPE);

void setup()
{
dht.begin();
Serial.begin(9600);

if (gsm.begin(9600))
{
Serial.println("\nstatus=READY");
started=true;
}
else
Serial.println("\nstatus=IDLE");
}

void loop()
{
float humidity, temperature;
String smsText ="";

switch (call.CallStatus())
{
case CALL_NONE: // Nothing is happening

break;

case CALL_INCOM_VOICE : //

Serial.println("RECEIVING CALL");
call.HangUp();
delay(2000);
humidity = dht.readHumidity();
temperature = dht.readTemperature();
delay(2000);
smsText = "Temperature: "+String(temperature,1)+"C Humidity: "+String(humidity,1)+"%";
smsText.toCharArray(sms_text,160);
//Serial.println(smsText);
sms.SendSMS("+4400000000",sms_text);
break;

case CALL_COMM_LINE_BUSY: //
Serial.println("TALKING. Line busy.");

break;
}
delay(1000);
}

Any help to do it with GPRSbee?

Thanks

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: GPRSbee rev.6

Post by kavi » Tue Dec 22, 2015 5:49 pm

The libraries in the gprs shield wiki can be used to implement your project.Please refer them in the following link.

Thanks and Regards

Post Reply