Page 1 of 1

XBee firmware configuration with X-CTU 6.2.0

Posted: Wed Dec 09, 2015 5:08 am
by georgiev1993
Hello,
I have two X-Bee S1 and I want to use them to read tempreture from a TMP36 sensor.To do this, I need to change the firmware of the 2 X-Bees. One of the X-Bees should be API Coordinator, the other one - AT Router.
However, I cannot upgrade the firmware of both XBees with the X-CTU software(version 6.2.0) The problem is that when I click on the upgrade firmware icon, there are only two product families - XB24 and XB24-DM. Neither of these families have the API Coordinator or the AT Router firmware. What should I do to put the desired functions to the 2 XBees?
Thank you for your reply.

Re: XBee firmware configuration with X-CTU 6.2.0

Posted: Mon Apr 25, 2016 11:39 am
by silver1row
Hello,

If you go to docs.digi and go to the Wireless Connectivity Kit and find the feedback section in the lower, right corner, you can send some bug related information when you click that feedback button.

There should be someone to answer this question, especially if it is XBee related. They have a pretty good customer service for their products.

Um...that is it. I wish you the best of luck.

Seth