Mesh Bee Firmware v1.0.4_preview

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
jephua
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Wed Sep 30, 2015 9:10 am

Mesh Bee Firmware v1.0.4_preview

Post by jephua » Wed Sep 30, 2015 9:12 am

Hi, I tried to flash the END_JN5168.bin in the output folder to the Mesh Bee and entered the MCU mode. I was expecting the heartbeat printout as shown in the code:

Code: Select all

    /* Air to Coordinator */
    uint16 size = i32CopyApiSpec(&apiSpec, tmp);
    if(API_bSendToAirPort(UNICAST, 0x0000, tmp, size))
    {
        suli_uart_printf(NULL, NULL, "<HeartBeat%d>\r\n", jobCnt);
        jobCnt++;
    }
But the serial monitor program did not show any result. Printing out the result of ZPS_eAplAfUnicastDataReq in the function API_bSendToAirPort results in error code 0xa6 - ZPS_APL_APS_E_INVALID_PARAMETER.

Anyone can help?

jephua
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Wed Sep 30, 2015 9:10 am

Re: Mesh Bee Firmware v1.0.4_preview

Post by jephua » Sat Oct 03, 2015 10:05 am

Anyone using Mesh Bee?

Post Reply