Bluetooth Bee Not saving settings

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
garth
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Mon Nov 05, 2012 10:19 pm

Bluetooth Bee Not saving settings

Post by garth » Mon May 20, 2013 9:46 pm

Hi

I have purchased a number of Bluetooth Bee modules, first about a year ago, and then recently.

When using the modules from a year ago everything works as expected. But when I use the recent modules I can set the Bluetooth Bee up, and it connects etc, but when I power down the system it loses all the settings I sent it.

Is this a firmware issue? What else could be causing this?

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Bluetooth Bee Not saving settings

Post by Jacket Chen » Tue May 21, 2013 3:57 pm

hi , the probability of fault happening may not be caused by the firmware, the firmware has been setted by the 'Default' settings,and we just upload the program to the bluetooth bee.

"+STAUTO=1" --- Permit Auto-connect. Save and Rest. (More information you can refer to the wiki:http://www.seeedstudio.com/wiki/index.p ... etooth_Bee)
Love little, love long.

Post Reply