Hello Everybody,
I have a problem with one bluetooth bee. I can't configure it. I use an UartSBee V4.0. I can connect with it and see some messages when device starts but I can't send any command (always returns ERROR). I tried SSCOM, hyperterm, putty and TeraTerm with the same results.
How must be done?
thanks so much
Configure Bluetooth Bee(Guidance)
Re: I can't configure Bluetooth Bee
Anybody can help me?
thanks
thanks
- Jacket Chen
- Staff
- Posts: 659
- Joined: Thu Jun 21, 2012 4:25 pm
- Are you a staff member of seeedstudio?: yes
- Which products/projects are your favorite?: Seeeduino Shields
- Location: China
Re: I can't configure Bluetooth Bee
How to configure Bluetooth Bee
hey , you can follow those steps:
1 Open sscom32 tool(picture 1),and you can find the EXT module,please click it.
2 And then you need add some commands to the blank(picture 2):
+STWMOD=0
+STNA=BTSlave
+STAUTO=0
+STOAUT=1
+STPIN=2222
+INQ=1
3 Now,we can send commands to bluetooth bee: 1) Please click 7(a blank command) 2) please click 1(+STWMOD=0),and then you can see the feedback of bluetooth bee(picture 4)
Note:If you click 1 first without clicking 7,you just get a error feedback(picture 3)
4 1) Please click 7(a blank command) 2) please click 2(+STNA=BTSlave)
5 1) Please click 7(a blank command) 2) please click 3(+STAUTO=0)
6 1) Please click 7(a blank command) 2) please click 4(+STOAUT=1)
7 1) Please click 7(a blank command) 2) please click 5(+STPIN=2222)
8 1) Please click 7(a blank command) 2) please click 6(+INQ=1)
When all steps have been done,then you can pair and connect your phone.(picture 5)
hey , you can follow those steps:
1 Open sscom32 tool(picture 1),and you can find the EXT module,please click it.
2 And then you need add some commands to the blank(picture 2):
+STWMOD=0
+STNA=BTSlave
+STAUTO=0
+STOAUT=1
+STPIN=2222
+INQ=1
3 Now,we can send commands to bluetooth bee: 1) Please click 7(a blank command) 2) please click 1(+STWMOD=0),and then you can see the feedback of bluetooth bee(picture 4)
Note:If you click 1 first without clicking 7,you just get a error feedback(picture 3)
4 1) Please click 7(a blank command) 2) please click 2(+STNA=BTSlave)
5 1) Please click 7(a blank command) 2) please click 3(+STAUTO=0)
6 1) Please click 7(a blank command) 2) please click 4(+STOAUT=1)
7 1) Please click 7(a blank command) 2) please click 5(+STPIN=2222)
8 1) Please click 7(a blank command) 2) please click 6(+INQ=1)
When all steps have been done,then you can pair and connect your phone.(picture 5)
Love little, love long.
Re: Configure Bluetooth Bee(Guidance)
FANTASTIC!!!
It works perfectly.
thanks so much
It works perfectly.
thanks so much
-
- Pre-kindergarten
- Posts: 20
- Joined: Sat Apr 27, 2013 9:48 pm
Re: Configure Bluetooth Bee(Guidance)
I can't get sscom32 to run on Windows 7 - and the other term programs I're tried are either no better or simply don't work.
I 'could' spin up a windows xp vm - read 'could' but really, should that be the way? I'm open to suggestions because I really need to get these bluetooth bees configured so they can be used to send data from the data loggers to a computer/phone.
I've tried compatibility mode - also not working and the same error every time.
help.
I 'could' spin up a windows xp vm - read 'could' but really, should that be the way? I'm open to suggestions because I really need to get these bluetooth bees configured so they can be used to send data from the data loggers to a computer/phone.
I've tried compatibility mode - also not working and the same error every time.
help.
Re: Configure Bluetooth Bee(Guidance)
HI,
I always used this soft in windows vista 32bits without problems. I never tested it in seven.
sorry
I always used this soft in windows vista 32bits without problems. I never tested it in seven.
sorry