Motor Driver 1.3, Problems with the voltage

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, salmanfarisvp, jeremy882, crail.lyu969

Post Reply
mightystanly
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Sun Sep 30, 2018 10:05 pm

Motor Driver 1.3, Problems with the voltage

Post by mightystanly » Sun Oct 07, 2018 11:34 pm

Hi,

i am using the motor driver 1.3. I have about 5V supply but at each motor there is only about 2V. Does the motor driver work like a voltage splitter?

Motor is a DC Brush, and Code looks like that, so maxmium power.

Motor.speed(MOTOR1, 100);
Motor.speed(MOTOR2, 100);

Any help? Regards.
stan

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Motor Driver 1.3, Problems with the voltage

Post by bill.yu » Tue Oct 16, 2018 3:16 pm

Hi Stan,

Working Voltage is 6~15V. please take a picture about the hardware connection. thanks.

Post Reply