Connect flow sensor to wio link

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
tachi
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Apr 04, 2016 8:25 pm

Connect flow sensor to wio link

Post by tachi » Mon Apr 04, 2016 8:32 pm

Hi,

I recently purchased a wio link which so far has been awesome.

I now want to attach a flow sensor https://www.seeedstudio.com/depot/G12-W ... p-635.html to it.

I am kind of new to this so excuse me if I am going down the wrong path.

I have the grove relay which I can turn on/off.

Would I strip the end of the wires on the flow sensor and have the red and black wire go into the relay.

How would I then connect the signal (yellow cable) to the wio to receive the flow data?

Any help would be great :)

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: Connect flow sensor to wio link

Post by kavi » Thu Apr 07, 2016 2:28 pm

Hi,

G1/2" Water Flow Sensor requires minimum 4.5V to operate and Wio Link can support only 3.3V so it does not support flow sensor.

Thanks and Regards

Post Reply