Grove NFC board not detected

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
chris.jones
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Nov 03, 2014 12:01 pm

Grove NFC board not detected

Post by chris.jones » Mon Nov 03, 2014 12:04 pm

I have the Grove NFC reader module and a Grove Mega Shield connected to an Arduino 2560 Mega.

Using Arduino 1.0.5.

I cut the UART to P1 trace and soldered P1 to I2C and verified that P1 and UART aren't connected with a voltmeter and also verified that P1 and I2C are connected.

I run the ReadTag example from NDEF library and I get the error:

Didn't find PN53x board.

I tried all 3 I2C ports on the Mega shield.

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Grove NFC board not detected

Post by Jacket Chen » Thu Nov 06, 2014 3:26 pm

We sincere apologised for that schematic problem, the I2C port of Grove - NFC has problem and we're solving it. We would put FAQ or solution on the wiki after we solve it. Sorry again and thanks for your comprehension.

Now only UART port can be used.

Jacket
Love little, love long.

schrubbi
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Tue Nov 25, 2014 4:41 pm

Re: Grove NFC board not detected

Post by schrubbi » Tue Nov 25, 2014 5:06 pm

Hi,
I've looked into the layout of the NFC board, and from what I've seen this is the problem:
The solder-jumper P1 is always connected to UART (meaning GND) and 'SEL0'

The NFC chip has 3 modes of communication, switched by the SEL0 and SEL1 level.
The correct usage is found here: www(dot)nxp(dot)com/documents/user_manual/141520.pdf (not allowed to post links -.-)

UART SEL0 0 | SEL1 0
SPI SEL0 0 | SEL1 1
I2C SEL0 1 | SEL1 0

So to be able to use I2C it is necessary to somehow unconnect the UART pad from the P1 jumper and then solder the jumper to the I2C pad.
Can someone confirm on that please?

Regards,
Chris

rburson
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Sep 22, 2014 11:24 pm

Re: Grove NFC board not detected

Post by rburson » Thu Feb 12, 2015 1:26 am

Jacket Chen wrote:We sincere apologised for that schematic problem, the I2C port of Grove - NFC has problem and we're solving it. We would put FAQ or solution on the wiki after we solve it. Sorry again and thanks for your comprehension.

Now only UART port can be used.

Jacket
Has this been fixed?!! Is it possible to use I2C with this board?

udaykiranruttala
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Feb 16, 2015 6:17 pm

Re: Grove NFC board not detected

Post by udaykiranruttala » Tue Feb 17, 2015 6:46 pm

I am facing the same problem. I am unable to interface grove nfc to ardunio UNO/Mega. as we have libraries written in I2C, I am unable to interface. can some one provide me libraries for interfacing grove nfc to arduino uno/mega using UART. Or libraries for interfacing grove nfc to ARM cortex M3 ( mbed). somebody please respond as soon as possible.

tanis666
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Mar 23, 2015 5:13 pm

Re: Grove NFC board not detected

Post by tanis666 » Mon Mar 23, 2015 5:46 pm

Hi,

I found a solution for I2C communication, it works on my two groove nfc modules.

The solution is:
- Remove the connection between P1 and UART
- Add a resistor 1 kOhm between P1 and the output of the regulator 3,3 V (no connection between P1 and I2C)
- Set Vcc at 5 V( with the pin 5 V of Arduino Uno), set gnd at 0 V (with the pin GND of ARduino Uno) and plug (RX,TX) to the pins (A5,A4)
- Use the example "ReadTag"
-Enjoy :)

R.Roder
University of Bordeaux
IUT Electronic - Indust. Info.
Last edited by Jacket Chen on Tue Mar 31, 2015 3:23 pm, edited 1 time in total.
Reason: +10 points. Good solution.

abehakanwal66
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Mar 27, 2015 3:56 pm

Re: Grove NFC board not detected

Post by abehakanwal66 » Fri Mar 27, 2015 4:01 pm

So to be able to use I2C it is necessary to somehow unconnect the UART pad from the P1 jumper and then solder the jumper to the I2C pad.
emma

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Grove NFC board not detected

Post by Jacket Chen » Tue Mar 31, 2015 3:27 pm

Sorry about this issue of schematic and thanks for tanis666 to put a solution here. Now we have solved this problem in a new version. Thanks for your comprehension.

Jacket
Love little, love long.

paintlax21
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Mon Mar 19, 2012 1:52 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: I don't have one

Re: Grove NFC board not detected

Post by paintlax21 » Mon May 11, 2015 9:27 am

I don't understand how to get this to work. Can anyone help me to get it working with an arduino uno?

Post Reply