Grove rotary encoder, push button function

Hello,

I am using a grove encoder (seeedstudio.com/wiki/Grove_-_Encoder) as a user interface device.

At the moment I am using a separate grove push button as the “action” input, but I would like to use the push function of the encoder.

I can’t find a pin out for the encoder, the documents in the wiki give the 3 pins ABC as the outputs for the encoder (and common).

Is it the two other pins on the opposite side?

Thank you in advance

answered my own question! check fault meters! :smiley:

For future reference: the two pins on the opposite side from the 3 rotary signal pins are a normally open switch (closed when pushed)