Arduino Ethernet + Grove Base Shield

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, salmanfarisvp, violet, jeremy882, crail.lyu969

Post Reply
mousefad
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Jan 12, 2013 2:35 pm

Arduino Ethernet + Grove Base Shield

Post by mousefad » Sat Jan 12, 2013 2:53 pm

Hi,

I would like to use the GROVE system base board with an Ethernet Arduino (with ethernet integrated with the arduino board). I understand that the Arduino Ethernet reserves a few pins for internal use... can someone confirm / refute that the GROVE base board works with the Arduino Ethernet?

Thanks
Mouse

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Arduino Ethernet + Grove Base Shield

Post by Jacket Chen » Mon Jan 14, 2013 2:55 pm

Hi,did you see a ICSP port on your Arduino(6pins port),but our base shield has no this port, and your ethernet need to plug into this port,so problem will occur when you are using our base shield with ethernet.....wow,i'm sorry , too wordy ....

in a word,you can use base shield , but solder a port on base shield firstly.
Love little, love long.

Post Reply