Grove I2C Motor Driver: stepper sample code, version number

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, salmanfarisvp, violet, jeremy882, crail.lyu969

Post Reply
dtr.vndrn
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Fri Jan 04, 2013 8:27 pm

Grove I2C Motor Driver: stepper sample code, version number

Post by dtr.vndrn » Fri Jan 04, 2013 8:43 pm

Hi,

I have bought the Grove I2C Motor Driver for controlling a stepper motor. The wiki only has sample code for DC motors. Is there code for a stepper?

Also, I received a board with v1.0 printed on the back (from Exp-tech in Germany). Is it outdated? If so, what are the differences with the current version?
Any problems to be expected in combination with an Arduino Uno and several other devices on the I2C bus?

Best, Dieter

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: Grove I2C Motor Driver: stepper sample code, version num

Post by Jacket Chen » Sun Jan 06, 2013 3:30 pm

Hi,we have no correspoding demo for stepper now,we'll fine it down later.

The latest version is v1.2.The v1.2 bring a stepper port and switch with it,but the function between them is the same.

Our base shield v1.3 is coming, it brings many I2C ports, UART ports with it,and you can use more devices via Base shield.
Love little, love long.

Post Reply