RGB LED Ring (20 and 24) 3D or 2D DWG/DXF file

Is it possible to publish a RGB LED Ring (24-WS2813 Mini) 3D or 2D DWG/DXF file. I need it for a CAD software.

Hi there~



Sorry to tell you that we actually don’t have any 3D or 2D DWG/DXF file. :frowning:



But the inner diameter is 53.30mm and the outer diameter is 70.30 mm.



Thanks cheers :smiley:



JL from Seeed.

Thanks. Can you please reply the inner and outer diameter of RGB LED Rings (20 and 24).

Hi



RGB LED Ring(20): inner diameter 43.00 mm and outer diameter 60.00 mm.



RGB LED Ring(24): inner diameter 53.30 mm and outer diameter 70.30 mm.



Thanks