Grove MCP9600 - changing device address?

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
jrgrohs
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Jul 04, 2019 11:08 pm

Grove MCP9600 - changing device address?

Post by jrgrohs » Thu Aug 15, 2019 10:29 pm

I would like to use two of the Grove MCP9600 sensors on the same I2C bus (I'm using a Lotus v1.1). I know that the two sensors will have the same addresses and that I need to change one of them. I see in the wiki where the address contacts are but I am not sure how I should alter them to have one of the sensors be on the alternate address.

Also, once this change has been made, what initialization changes are needed to then use two sets of functions throughout my code (i.e., get_temperature1() and get_temperature2())

Thanks for any help you can offer!

~JRG

bill.yu
Junior-7
Junior-7
Posts: 732
Joined: Mon Apr 02, 2018 11:05 am

Re: Grove MCP9600 - changing device address?

Post by bill.yu » Tue Aug 20, 2019 4:46 pm

Hi JRG~

You can use the software I2C, connect the sensor to digital port of the lotus1.1. I will talk with software team and modify the library to enable this function. Keep you posted. thanks.

jrgrohs
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Jul 04, 2019 11:08 pm

Re: Grove MCP9600 - changing device address?

Post by jrgrohs » Wed Aug 21, 2019 11:10 pm

Great - thanks!

Post Reply