Grove - Voltage Divider

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
matthias.schmidt
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Thu Aug 01, 2019 4:40 pm

Grove - Voltage Divider

Post by matthias.schmidt » Thu Aug 01, 2019 4:44 pm

Is it possible to use the Voltage Divider for input signal of -10 to +10 V and scale to 0 to 10 V?

bill.yu
Junior-7
Junior-7
Posts: 732
Joined: Mon Apr 02, 2018 11:05 am

Re: Grove - Voltage Divider

Post by bill.yu » Fri Aug 02, 2019 2:43 pm

Hi there~

The max input is 1V~43V and max output is 5V. You can refer to below link for more detail. thanks.

http://wiki.seeedstudio.com/Grove-Volta ... cification

Post Reply