Grove High temperature sensor values, can you help

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Wed Jun 05, 2019 10:59 am

Grove High temperature sensor values, can you help
I need to be able to extract resistance a, room temp and the temp read by the sensor. I dont know what the functions are or what they do.

I want to know what these do and have access to them so that I can use them in my program, but they are function.

I bought my staff through Arduino.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Wed Jun 05, 2019 5:48 pm

Hi there,

1. The blue dot on the board reads the room temperature, which is used for the high temperature sensor calibration.



3. We covert the voltage to temperature.

4. Add the room temperature as offset and calculate the high temperature. 

Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Fri Jun 07, 2019 7:14 am

Hi Bill and team,

Thank you fo ryour response, I will look into the information and get back to you once I have tried the info.

The question that I ahve at the moment is. What does the the temperature sensor read then since the thermisoe(blue dot) measures room temp.
I basicall need something that will measure the temperature inside a car and I can data log that using Arduino. Can you help with this?
Regards,

Mthulisi

Sent from Mail for Windows 10

Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Sun Jun 09, 2019 11:54 am

HI Bill,

Thank you for taking time to respond to my request and for uploading the links that you made.
I however am having the problems in uploading them in the Arduino. Please find the attached screen shot.
Regards,
Mthulisi


Sent from Mail for Windows 10

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Tue Jun 11, 2019 2:33 pm

Hi there,

What i provided previously is the library, NOT the example code. 

You can use this example.


Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Wed Jun 26, 2019 11:08 am

Hi Bill,

Thank you. I do understand. What I was hopping to get is the Room temperature so that I can do this to the code.

Serial.print(roomTemp); This way I can do conditional statements to say
If roomTemp is == ***

Then_ _

So in other words it is not possible to extract this from the programs. But hte room temperature can be seen from the start of the program, but it is a fucntion, so once can not do the
Serial.print(roomTemp); ...


On another note, please hele with the libraries listed in the attached document. I need to buy you other sensor that works with that program.
Regards,


Mthulisi Mlilo

Sent from Mail for Windows 10

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Wed Jun 26, 2019 2:07 pm

Hi 

Mthulisi,  

1. For the High temperature sensor, it uses to measure high temperature up to 600 degree C. If you want to use to measure the temperature inside card, you can use normal temperature sensor. 

You can connect the sensor to A0 port of base shield, which includes a0 and a1 pins. If you do not have base shield, you can follow below connection.























SeeeduinoGrove-High Temperature Sensor
GNDBlack
5VRed
A1White
A0Yellow




 
#include "High_Temp.h"



HighTemp ht(A1, A0);

void setup()
{
    Serial.begin(115200);
    Serial.println("grove - hight temperature sensor test demo");
    ht.begin();
}

void loop()
{
    Serial.println(ht.getThmc()); //high temp
    Serial.println(ht.getRoomTmp()); //room temp
    delay(100);
}


2. For the grove temp sensor, thanks for the inputs, I will update the wiki. 


Thanks

best rgds
Bill


Post Reply