can you please tell me what the Max ratings on the input pins IP+ and IP- are of sensors ACS70331 and ACS725 are

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

can you please tell me what the Max ratings on the input pins IP+ and IP- are of sensors ACS70331 and ACS725 are

Post by Anonymous » Fri May 17, 2019 5:26 pm

Hi, can you please tell me what the Max ratings on the input pins IP+ and IP- are of sensors ACS70331 and ACS725 are? I need to measure the current consumption (Typically 0 to 4 Amp DC) of a 48V DC unit.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Mon May 20, 2019 9:45 am

Hi there,

You can consider to use below product, 

http://wiki.seeedstudio.com/Grove-5A_DC ... -ACS70331/  

Parameter
Value



Supply voltage
3.3V / 5V


Operating ambient temperature
-40 – 85?


Storage temperature
- 65°C – 125°C


Working Voltage
<100V


Current sensing range
0 – 5A


Sensitivity
200mV/A(Typ.)


Output interface
Grove Analog


Input interface
Screw terminal

Post Reply