Multiple Capacitive Touch Slide Sensors (CY8C) Through I2C on Arduino

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
rkarst15
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Apr 05, 2019 4:12 pm

Multiple Capacitive Touch Slide Sensors (CY8C) Through I2C on Arduino

Post by rkarst15 » Fri Apr 05, 2019 4:19 pm

Hi !

I want to connect three cy8c sliders to an arduino through i2c ports (and be able to separate them into three data streams). I am using the Base Shield v2 which gives me 4 i2c ports.

When I am using one cy8c with the demo for ardunio, it works perfectly fine. However, when i connect two, neither of them sends any data.

I am guessing that i should change the default i2c address for the different sliders, is this possible with the cy8c? And how do you do that then?

Hope someone can help me !

Thanks in advance.

- I2C noob

Post Reply