Page 1 of 1

Music Shield and Wiznet Ethernet shield

Posted: Fri Mar 30, 2012 2:28 pm
by genhung
Hi there,

I have just received the following items from Seeed Studio

(1) Music Shield (INT109B2P)
(2) Wiznet Ethernet shield -w5100 (ARD124B2P)

Are these two boards compatible to each other?
How can I joint them together onto an Arduino MEGA board?

Please help.

Re: Music Shield and Wiznet Ethernet shield

Posted: Sat Mar 31, 2012 12:01 pm
by deray
Hi~
You can try to weld Female header on the Wiznet Ethernet shield.Hope this help to you.


Best regards,
deray

Re: Music Shield and Wiznet Ethernet shield

Posted: Sat Mar 31, 2012 1:33 pm
by genhung
thanks deray
It sounds to me I can put Ethernet shield on the MEGA, then MUSIC shield on the Ether shield. Is it?
Is it fine for not connecting ISP (6pin::MISO\SCK\RST\VCC\HOSI\GND) to Music Shield??
Thanks again!

Re: Music Shield and Wiznet Ethernet shield

Posted: Sat Mar 31, 2012 2:17 pm
by deray
Yes,it is.
ISP interface is kept for bringing SPI port when using with Mega , so you should be connected it to MEGA ISP .

best regards,
deray

Re: Music Shield and Wiznet Ethernet shield

Posted: Wed Apr 04, 2012 9:56 am
by genhung
hi deray

If both Music Shield and Wiznet Ethernet shield need ISP interface for talking to MEGA,
When I joint these two shield together, will it cause conflicts???

Thanks

Re: Music Shield and Wiznet Ethernet shield

Posted: Mon Apr 09, 2012 10:24 am
by deray
yeah,you can joint these two shield together. but you must change the on of the D10 (Used for SPI Chip Select.pin) , because both of them use the same chip select.ping.